<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: UART on kl25z in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-on-kl25z/m-p/296733#M12230</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Aayush&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;UART0 is a special UART module. It can support basic UART with DMA interface function, x4 to x32 oversampling of baud-rate.This module supports LIN slave operation.&lt;/P&gt;&lt;P&gt;The module can remain functional in VLPS mode provided the clock it is using remains enabled. It can support ISO7816.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;UART1 and UART2 are basic universal asynchronous receiver/transmitter (UART) modules with DMA function support. Generally, these modules are used in RS-232, RS-485, and other communications. This module supports LIN Slave operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;UART pins are digital. So the operation voltage depends on VDD voltage value.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope my reply can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Mar 2014 04:12:11 GMT</pubDate>
    <dc:creator>Paul_Tian</dc:creator>
    <dc:date>2014-03-17T04:12:11Z</dc:date>
    <item>
      <title>UART on kl25z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-on-kl25z/m-p/296732#M12229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the differnce&amp;nbsp; between UART0, UART1, UART2 on kl25z ?&lt;/P&gt;&lt;P&gt;What is the operating voltage of RX/TX pin of kl25z ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Mar 2014 19:57:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-on-kl25z/m-p/296732#M12229</guid>
      <dc:creator>aayushm</dc:creator>
      <dc:date>2014-03-14T19:57:41Z</dc:date>
    </item>
    <item>
      <title>Re: UART on kl25z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-on-kl25z/m-p/296733#M12230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Aayush&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;UART0 is a special UART module. It can support basic UART with DMA interface function, x4 to x32 oversampling of baud-rate.This module supports LIN slave operation.&lt;/P&gt;&lt;P&gt;The module can remain functional in VLPS mode provided the clock it is using remains enabled. It can support ISO7816.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;UART1 and UART2 are basic universal asynchronous receiver/transmitter (UART) modules with DMA function support. Generally, these modules are used in RS-232, RS-485, and other communications. This module supports LIN Slave operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;UART pins are digital. So the operation voltage depends on VDD voltage value.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope my reply can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Mar 2014 04:12:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-on-kl25z/m-p/296733#M12230</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2014-03-17T04:12:11Z</dc:date>
    </item>
  </channel>
</rss>