<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: FRDM-K20D50M not running pre-compiled examples</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K20D50M-not-running-pre-compiled-examples/m-p/295859#M12187</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the help so far.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I'm trying to download the file to the drive when it is in "FRDM-K20D50" mode. However, when it is in BOOTLOADER mode I am able to send the system files correctly without getting any error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm talking to pemicro support and aparently error 7 means communication error (I hoped that it would be a bit more specific). I hope it is somehow a software problem because I just received the board and really want to start working with it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 May 2014 20:28:45 GMT</pubDate>
    <dc:creator>joaolugao</dc:creator>
    <dc:date>2014-05-13T20:28:45Z</dc:date>
    <item>
      <title>FRDM-K20D50M not running pre-compiled examples</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K20D50M-not-running-pre-compiled-examples/m-p/295855#M12183</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I just recieved my FRDM-K20D50M board and I'm having trouble with the pre-compiled examples. So far I've tried updating the bootloader, downloading the file MSD-DEBUG-FRDM-K20D50M_Pemicro_v114.SDA to the bootloader of the device and nothing seems to work. I have tried to do this both in windows 8 and windows 7.&lt;/P&gt;&lt;P&gt;When I download an example to the device it stops running the sample code that come with it (blinking the RGB led) and leave a static blue led on. When I press reset nothing happens. sometimes the laststat will show Error 7 and sometimes ready. When I unplug and plug the USB again the original sample code will start running again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FYI&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Arial, Helvetica, sans-serif; font-size: small; background-color: #c2d1f0;"&gt;Board Name is: FRDM-K20D50M&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Arial, Helvetica, sans-serif; font-size: small; background-color: #c2d1f0;"&gt;MicroBoot Kernel Version is: 1.03&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Arial, Helvetica, sans-serif; font-size: small; background-color: #c2d1f0;"&gt;Bootloader Version is: 1.11&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Arial, Helvetica, sans-serif; font-size: small; background-color: #c2d1f0;"&gt;Installed Application: PEMicro FRDM-K20D50M Mass Storage/Debug App&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Arial, Helvetica, sans-serif; font-size: small; background-color: #c2d1f0;"&gt;Application Version is: 1.14&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anybody help me? or is my board DOA?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 May 2014 23:15:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K20D50M-not-running-pre-compiled-examples/m-p/295855#M12183</guid>
      <dc:creator>joaolugao</dc:creator>
      <dc:date>2014-05-12T23:15:03Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K20D50M not running pre-compiled examples</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K20D50M-not-running-pre-compiled-examples/m-p/295856#M12184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Joao&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You didn't say how you were trying to download code to the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the same board and the only difference that I can see is that your has a newer Bootloader version (1.11 instead of 1.05, as mine has).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Presumably the board is appearing as a hard drive to your PC. If this is the case, try dragging and dropping the binary file that I have attached to see whether it runs. I have just tested it on my board by using the same method. It is copied and starts up with no further action needed.&lt;/P&gt;&lt;P&gt;If it runs (LED flashes and varies in colour), you can communicate with the UART via the virtual COM port and you will see a menu (115kBaud) which has various menu points that can be used to test the board (including the accelerometer, the LED colours and even testing reading/writing/erasing areas or program flash or FlexNVM).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 May 2014 01:48:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K20D50M-not-running-pre-compiled-examples/m-p/295856#M12184</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-05-13T01:48:55Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K20D50M not running pre-compiled examples</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K20D50M-not-running-pre-compiled-examples/m-p/295857#M12185</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the reply. I've tried dragging and dropping the binary file as described. Right at the time the file transfer begins the green led starts flashing 8 times and pausing 2 seconds indicating error, this happens every time I try to drag and drop without being in the bootloader mode. The LASTSTAT file says error 7.&lt;/P&gt;&lt;P&gt;I was trying to program by dragging and dropping the precompiled codes to the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Joao&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 May 2014 02:04:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K20D50M-not-running-pre-compiled-examples/m-p/295857#M12185</guid>
      <dc:creator>joaolugao</dc:creator>
      <dc:date>2014-05-13T02:04:58Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K20D50M not running pre-compiled examples</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K20D50M-not-running-pre-compiled-examples/m-p/295858#M12186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Joao&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Make sure that when you load an application you don't hold the reset button down when attaching the USB.&lt;/P&gt;&lt;P&gt;- When holding it down the hard drive appears as "BOOTLOADER"&lt;BR /&gt;- When the button is not held, the drive appears as "FRDM-K20D50"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When in the "BOOTLOADER" any SW upload will go to the K20 that is used as debug interface.&lt;/P&gt;&lt;P&gt;Only in "FRDM-K20D50 loader mode will the loaded code go to the K20 that is there for development use.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible that you have been loading always in BOOTLOADER mode?&lt;BR /&gt;I did in fact try copying the attached code to the BOOTLOADER and it accepted it without error in the "LASTSTAT.TXT" (and I needed to reload the original SDA to get the debugger working again) so it does sound more like a problem with the board or the boot loader version - I would contact P&amp;amp;E to find out what the error code means - &lt;A href="http://www.pemicro.com/opensda/index.cfm" title="http://www.pemicro.com/opensda/index.cfm"&gt;http://www.pemicro.com/opensda/index.cfm&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 May 2014 03:22:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K20D50M-not-running-pre-compiled-examples/m-p/295858#M12186</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-05-13T03:22:37Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K20D50M not running pre-compiled examples</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K20D50M-not-running-pre-compiled-examples/m-p/295859#M12187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the help so far.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I'm trying to download the file to the drive when it is in "FRDM-K20D50" mode. However, when it is in BOOTLOADER mode I am able to send the system files correctly without getting any error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm talking to pemicro support and aparently error 7 means communication error (I hoped that it would be a bit more specific). I hope it is somehow a software problem because I just received the board and really want to start working with it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 May 2014 20:28:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K20D50M-not-running-pre-compiled-examples/m-p/295859#M12187</guid>
      <dc:creator>joaolugao</dc:creator>
      <dc:date>2014-05-13T20:28:45Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K20D50M not running pre-compiled examples</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K20D50M-not-running-pre-compiled-examples/m-p/295860#M12188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Joao,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check below link, P&amp;amp;E provides updated OPENSDA firmware, the MSD firmware version is MSD-DEBUG-FRDM-K20D50M_Pemicro_v114. You could download it from below link:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.pemicro.com/opensda/index.cfm"&gt;http://www.pemicro.com/opensda/index.cfm&lt;/A&gt;&lt;/P&gt;&lt;P&gt;When there shows "FRDM-K20D50" disk, you could drag and drop the Precompiled example image file to this disk, then the example demo will run.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 May 2014 05:33:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K20D50M-not-running-pre-compiled-examples/m-p/295860#M12188</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2014-05-14T05:33:45Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K20D50M not running pre-compiled examples</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K20D50M-not-running-pre-compiled-examples/m-p/295861#M12189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This was apparently a problem with MSD application for FRDM-K20D50M.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For those experiencing this issue, P&amp;amp;E created a new fixed version (&lt;STRONG&gt;MSD-DEBUG-FRDM-K20D50M_Pemicro_v115.SDA&lt;/STRONG&gt;) which is included in the latest OpenSDA Firmware Apps package. The link to download is below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/opensda"&gt;www.pemicro.com/opensda&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Sep 2014 00:25:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K20D50M-not-running-pre-compiled-examples/m-p/295861#M12189</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-09-06T00:25:32Z</dc:date>
    </item>
  </channel>
</rss>