<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 SMAC @ 433MHz</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SMAC-433MHz/m-p/295773#M12181</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I'm developing a MRB-KW01 application at 433 MHz, but the SMAC source code provided with "radio utility GUI" is an application example only for 868 and 960 MHz. &lt;/P&gt;&lt;P&gt;Is there any source code for 433 MHz band? Or maybe I've just to change manually radio parameters?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 May 2014 14:31:50 GMT</pubDate>
    <dc:creator>mircopizzichini</dc:creator>
    <dc:date>2014-05-12T14:31:50Z</dc:date>
    <item>
      <title>SMAC @ 433MHz</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SMAC-433MHz/m-p/295773#M12181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I'm developing a MRB-KW01 application at 433 MHz, but the SMAC source code provided with "radio utility GUI" is an application example only for 868 and 960 MHz. &lt;/P&gt;&lt;P&gt;Is there any source code for 433 MHz band? Or maybe I've just to change manually radio parameters?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 May 2014 14:31:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SMAC-433MHz/m-p/295773#M12181</guid>
      <dc:creator>mircopizzichini</dc:creator>
      <dc:date>2014-05-12T14:31:50Z</dc:date>
    </item>
    <item>
      <title>Re: SMAC @ 433MHz</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SMAC-433MHz/m-p/295774#M12182</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello mircopizzichini, &lt;/P&gt;&lt;P&gt;You are correct in the fact that SMAC doesn't currently provide support for 433MHz band.&lt;/P&gt;&lt;P&gt;What you can do is the following:&lt;/P&gt;&lt;P&gt;In RadioUtility.h set the default settings that you need to run @ 433MHz.&lt;/P&gt;&lt;P&gt;You need to calculate the Frf registers value for the 433MHz.&lt;/P&gt;&lt;P&gt;The formula is:&lt;/P&gt;&lt;P&gt;Frf Register= Frf/Fstep&lt;/P&gt;&lt;P&gt;where Fstep=FXosc/2^19&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;current value:&lt;/P&gt;&lt;P&gt;#define gDefaultRfFreq_c ( 0xE4C000 )&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //rf freq 915 MHz (US).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;desired value for 433MHz:&lt;/P&gt;&lt;P&gt;#define gDefaultRfFreq_c ( 0x6C4000 )&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //rf freq 433 MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you need to change other parameters such as Fdev, BitRate, and so on you can do it in RadioUtility.h as well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 May 2014 20:08:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SMAC-433MHz/m-p/295774#M12182</guid>
      <dc:creator>CesarM</dc:creator>
      <dc:date>2014-05-12T20:08:44Z</dc:date>
    </item>
  </channel>
</rss>