<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MKW01xx DIO0 and DIO1 ,,enhanced performance'' in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW01xx-DIO0-and-DIO1-enhanced-performance/m-p/295531#M12149</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you for clarification, yet it is still unclear to me, why I have to route them specifically to PTC4 and PTC3 (or why not just pull them up/down internally on PTE).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Pavel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Mar 2014 10:09:06 GMT</pubDate>
    <dc:creator>pkral</dc:creator>
    <dc:date>2014-03-20T10:09:06Z</dc:date>
    <item>
      <title>MKW01xx DIO0 and DIO1 ,,enhanced performance''</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW01xx-DIO0-and-DIO1-enhanced-performance/m-p/295529#M12147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From MKW01xx Reference Manual, Rev. 2:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;4.4.1 Additional Transceiver Status Signals&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MKW01Z128 transceiver has a total of six outputs (DIO5:DIO0) that can be programmed as status&amp;nbsp; &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;indicators:&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;DIO1 and DIO0 are connected to MCU GPIOs, PTE3 &amp;amp; PTE2, internally to the package. For &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;certain software configurations, &lt;STRONG&gt;improved performance can be obtained by connecting to &lt;/STRONG&gt;&lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;STRONG&gt;additional GPIOs, PTC4, and PTC3, off chip.&lt;/STRONG&gt; These connections are used by applications software &lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;in packet mode.&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does it mean use of LLWU (i.e.SyncAddress, CrcOk,... ) on PTC4, PTC3 to wake up sleeping MCU when transceiver do radio RX duty cycling or anything else ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Pavel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Mar 2014 15:23:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW01xx-DIO0-and-DIO1-enhanced-performance/m-p/295529#M12147</guid>
      <dc:creator>pkral</dc:creator>
      <dc:date>2014-03-13T15:23:16Z</dc:date>
    </item>
    <item>
      <title>Re: MKW01xx DIO0 and DIO1 ,,enhanced performance''</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW01xx-DIO0-and-DIO1-enhanced-performance/m-p/295530#M12148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It mean that if you want to use &lt;STRONG&gt;DIO1&lt;/STRONG&gt; and &lt;STRONG&gt;DIO0&lt;/STRONG&gt; in enhanced mode, you should route these signals to PTC4 &amp;amp; PTC3 pins, instead use them on default pins (PTE3 &amp;amp; PTE2).&lt;/P&gt;&lt;P&gt;The reason for this is explained on &lt;STRONG&gt;8.1 LGA Package Maximum Ratings&lt;/STRONG&gt; in the datasheet &lt;A href="http://cache.freescale.com/files/microcontrollers/doc/data_sheet/MKW01Z128.pdf?fpsp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;Parent_nodeId=1348518959280720745857&amp;amp;Parent_pageType=product"&gt;&lt;STRONG&gt;MKW01Z128&lt;/STRONG&gt;&lt;/A&gt;:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;This device contains circuitry protecting against damage due to high static voltage or electrical fields;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;however, it is advised that normal precautions be taken to avoid application of any voltages higher than&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;maximum-rated voltages to this high-impedance circuit. Reliability of operation is enhanced if unused&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;inputs are tied to an appropriate logic voltage level (for instance, either VSS or VDD) or the programmable&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;pull-up resistor associated with the pin is enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a nice day :P,&lt;BR /&gt;Perla&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Mar 2014 23:11:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW01xx-DIO0-and-DIO1-enhanced-performance/m-p/295530#M12148</guid>
      <dc:creator>perlam_i_au</dc:creator>
      <dc:date>2014-03-19T23:11:56Z</dc:date>
    </item>
    <item>
      <title>Re: MKW01xx DIO0 and DIO1 ,,enhanced performance''</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW01xx-DIO0-and-DIO1-enhanced-performance/m-p/295531#M12149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you for clarification, yet it is still unclear to me, why I have to route them specifically to PTC4 and PTC3 (or why not just pull them up/down internally on PTE).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Pavel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Mar 2014 10:09:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW01xx-DIO0-and-DIO1-enhanced-performance/m-p/295531#M12149</guid>
      <dc:creator>pkral</dc:creator>
      <dc:date>2014-03-20T10:09:06Z</dc:date>
    </item>
    <item>
      <title>Re: MKW01xx DIO0 and DIO1 ,,enhanced performance''</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW01xx-DIO0-and-DIO1-enhanced-performance/m-p/295532#M12150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pavel:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know the meaning of that "improved performance", but yes, I suppose you could use those flags (SyncAddress, CrcOk, FifoFull, FifoNotEmpty, etc) as wake-up sources, as long as you configure properly the LLWU unit of the internal MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, as for why it says specifically PTC3 and PTC4, I think this is because of the connections in the Modular Reference Boards (&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MRB-KW0x&amp;amp;parentCode=KW0x&amp;amp;fpsp=1" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MRB-KW0x&amp;amp;parentCode=KW0x&amp;amp;fpsp=1"&gt;MRB-KW0x: Modular Reference Boards for Kinetis KW0x Family of MCUs&lt;/A&gt;). Check this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43288iA95A2FC98D35C906/image-size/large?v=v2&amp;amp;px=999" title="DIO_0_1.png" alt="DIO_0_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Mar 2014 14:23:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW01xx-DIO0-and-DIO1-enhanced-performance/m-p/295532#M12150</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-03-21T14:23:23Z</dc:date>
    </item>
  </channel>
</rss>