<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Exit K20D50  from LLS mode to active mode using UART RX pin to enable LLWU in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Exit-K20D50-from-LLS-mode-to-active-mode-using-UART-RX-pin-to/m-p/295294#M12124</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Exactly, it is. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Apr 2014 03:23:21 GMT</pubDate>
    <dc:creator>joginderrana</dc:creator>
    <dc:date>2014-04-15T03:23:21Z</dc:date>
    <item>
      <title>Exit K20D50  from LLS mode to active mode using UART RX pin to enable LLWU</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Exit-K20D50-from-LLS-mode-to-active-mode-using-UART-RX-pin-to/m-p/295292#M12122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am facing a problem in exiting k20d50 controller from the LLS mode to active mode. I did it using external LLWU GPIO pin. But for a certain application I need to enable LLWU mode by pulling the UART RX line active high. &lt;/P&gt;&lt;P&gt;This feature is given in the K20 Sub-Family Reference Manual (page number 67). I am just wondering to know how to activate this mode in MK20DX128VLH5 MCU.&amp;nbsp; I am using cw-10.5 and is equipped with processor expert.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Apr 2014 05:27:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Exit-K20D50-from-LLS-mode-to-active-mode-using-UART-RX-pin-to/m-p/295292#M12122</guid>
      <dc:creator>joginderrana</dc:creator>
      <dc:date>2014-04-14T05:27:07Z</dc:date>
    </item>
    <item>
      <title>Re: Exit K20D50  from LLS mode to active mode using UART RX pin to enable LLWU</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Exit-K20D50-from-LLS-mode-to-active-mode-using-UART-RX-pin-to/m-p/295293#M12123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I noticed this is a replication from &lt;A href="https://community.nxp.com/thread/322348"&gt;Exit K20D50&amp;nbsp; from LLS mode active mode using UART RX pin to enable LLWU&lt;/A&gt; this other thread I will assume ignore the one I mentioned, and assume this is the&amp;nbsp; "good one"ok?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Apr 2014 19:50:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Exit-K20D50-from-LLS-mode-to-active-mode-using-UART-RX-pin-to/m-p/295293#M12123</guid>
      <dc:creator>perlam_i_au</dc:creator>
      <dc:date>2014-04-14T19:50:43Z</dc:date>
    </item>
    <item>
      <title>Re: Exit K20D50  from LLS mode to active mode using UART RX pin to enable LLWU</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Exit-K20D50-from-LLS-mode-to-active-mode-using-UART-RX-pin-to/m-p/295294#M12124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Exactly, it is. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Apr 2014 03:23:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Exit-K20D50-from-LLS-mode-to-active-mode-using-UART-RX-pin-to/m-p/295294#M12124</guid>
      <dc:creator>joginderrana</dc:creator>
      <dc:date>2014-04-15T03:23:21Z</dc:date>
    </item>
    <item>
      <title>Re: Exit K20D50  from LLS mode to active mode using UART RX pin to enable LLWU</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Exit-K20D50-from-LLS-mode-to-active-mode-using-UART-RX-pin-to/m-p/295295#M12125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You mention you have successfully used &lt;STRONG&gt;LLWU&lt;/STRONG&gt; module to get out from &lt;STRONG&gt;LLS&lt;/STRONG&gt; mode by external pin trigger but now you would like to do the same but using a UART_RX signal instead external signal trigger, as it's mentioned on &lt;STRONG&gt;AWIC&lt;/STRONG&gt; module but I am afraid this is not possible because the &lt;STRONG&gt;LLWU&lt;/STRONG&gt; module has been designed specifically to wake up from &lt;STRONG&gt;LLS&lt;/STRONG&gt; mode and &lt;STRONG&gt;AWIC&lt;/STRONG&gt; module has been designed to get out from &lt;STRONG&gt;STOP&lt;/STRONG&gt; and &lt;STRONG&gt;VLPS&lt;/STRONG&gt; modes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please verify this information on diagrams which describe the interactions for &lt;STRONG&gt;LLWU&lt;/STRONG&gt; (&lt;EM&gt;Figure 16-1. LLWU block diagram&lt;/EM&gt;) and &lt;STRONG&gt;AWIC&lt;/STRONG&gt; (&lt;EM&gt;Figure 9-1. Cortex-M4 Debug Topology&lt;/EM&gt;) in the reference manual &lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/K20P64M50SF0RM.pdf"&gt;&lt;STRONG&gt;K20P64M50SF0RM&lt;/STRONG&gt;&lt;/A&gt;. You will notice that wake up sources from &lt;STRONG&gt;AWIC&lt;/STRONG&gt; (&lt;EM&gt;Table 3-7. AWIC Stop and VLPS Wake-up Sources&lt;/EM&gt;) are completely different from wake up sources of &lt;STRONG&gt;LLWU&lt;/STRONG&gt; (&lt;EM&gt;Table 3-13. Wakeup sources for LLWU inputs&lt;/EM&gt;).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if this information is useful or if I have understood your issue.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a nice day :P,&lt;BR /&gt;Perla&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Apr 2014 21:42:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Exit-K20D50-from-LLS-mode-to-active-mode-using-UART-RX-pin-to/m-p/295295#M12125</guid>
      <dc:creator>perlam_i_au</dc:creator>
      <dc:date>2014-04-16T21:42:06Z</dc:date>
    </item>
  </channel>
</rss>