<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: TWR-K64F120 can not be connected?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K64F120-can-not-be-connected/m-p/295262#M12103</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would check that the OpenSDA software installed is correct for debugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Go to the P&amp;amp;E site and download the latest Pemicro OpenSDA debug update apps: &lt;A href="http://www.pemicro.com/opensda/index.cfm" title="http://www.pemicro.com/opensda/index.cfm"&gt;P&amp;amp;E Microcomputer Systems&lt;/A&gt;&lt;/P&gt;&lt;P&gt;There is one for your board called &lt;STRONG&gt;MSD-DEBUG-TWR-K64F120_Pemicro_v114.SDA&lt;/STRONG&gt; and if you upgrade to this one (according to the details on that page) you may find it then works.&lt;/P&gt;&lt;P&gt;For some reason the boards are delivered with a Mass Storage loader programmed (it does say Mass Storage / Debug App above but I don't think that it means that it can be used as debugger (?). I have about 10 boards with OpenSDA and had to reprogram all of them first to be able to work with the debugger - after programming (which is thankfully simple) all worked fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note for people who use Rowely Crossworks: this IDE used &lt;STRONG&gt;CMSIS-DAP_OpenSDA.S19 &lt;/STRONG&gt;which is contained in contained in the KL25 quickstart package - see &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KL25Z" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KL25Z"&gt;FRDM-KL25Z: Freescale Freedom Development Platform for Kinetis KL14/15/24/25 MCUs&lt;/A&gt; I believe the single file is suitable for all processors (but not fully sure at the moment since I only tested it on the KL25 'till now).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Mar 2014 19:26:00 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2014-03-13T19:26:00Z</dc:date>
    <item>
      <title>TWR-K64F120 can not be connected?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K64F120-can-not-be-connected/m-p/295261#M12102</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I just got a TWR-K64F120 for the larger RAM.&lt;/P&gt;&lt;P&gt;I installed the Freescale_MQX_4_0_TWRK64F120M.&lt;/P&gt;&lt;P&gt;When I try to download the hello sample code to it through OpenSDA, it does not work.&lt;/P&gt;&lt;P&gt;&lt;IMG alt="" /&gt;&lt;/P&gt;&lt;P&gt;&lt;IMG alt="" /&gt;&lt;/P&gt;&lt;P&gt;&lt;IMG alt="" src="https://community.nxp.com/" /&gt;&lt;/P&gt;&lt;P&gt;When I checked the OpenSDA information, it shows&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43166i7F3EAD368C7CD681/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the link &lt;A href="http://mcuoneclipse.com/2014/03/02/first-steps-with-the-freescale-twr-k64f120m/#more-10887" title="http://mcuoneclipse.com/2014/03/02/first-steps-with-the-freescale-twr-k64f120m/#more-10887"&gt;First Steps with the Freescale TWR-K64F120M | MCU on Eclipse&lt;/A&gt;, I also tried connect J39, but it still does not work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I tried to use the Multilink Universal Debugger, no matter with J39 and J16 connected or not, it shows&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43167iE88BB2FFD0B777E6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and sometime the power LED is not on the LED D3 is blinking.&lt;/P&gt;&lt;P&gt;I am confused.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any one has some ideas about this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Mar 2014 13:09:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K64F120-can-not-be-connected/m-p/295261#M12102</guid>
      <dc:creator>danielchai</dc:creator>
      <dc:date>2014-03-13T13:09:14Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K64F120 can not be connected?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K64F120-can-not-be-connected/m-p/295262#M12103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would check that the OpenSDA software installed is correct for debugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Go to the P&amp;amp;E site and download the latest Pemicro OpenSDA debug update apps: &lt;A href="http://www.pemicro.com/opensda/index.cfm" title="http://www.pemicro.com/opensda/index.cfm"&gt;P&amp;amp;E Microcomputer Systems&lt;/A&gt;&lt;/P&gt;&lt;P&gt;There is one for your board called &lt;STRONG&gt;MSD-DEBUG-TWR-K64F120_Pemicro_v114.SDA&lt;/STRONG&gt; and if you upgrade to this one (according to the details on that page) you may find it then works.&lt;/P&gt;&lt;P&gt;For some reason the boards are delivered with a Mass Storage loader programmed (it does say Mass Storage / Debug App above but I don't think that it means that it can be used as debugger (?). I have about 10 boards with OpenSDA and had to reprogram all of them first to be able to work with the debugger - after programming (which is thankfully simple) all worked fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note for people who use Rowely Crossworks: this IDE used &lt;STRONG&gt;CMSIS-DAP_OpenSDA.S19 &lt;/STRONG&gt;which is contained in contained in the KL25 quickstart package - see &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KL25Z" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KL25Z"&gt;FRDM-KL25Z: Freescale Freedom Development Platform for Kinetis KL14/15/24/25 MCUs&lt;/A&gt; I believe the single file is suitable for all processors (but not fully sure at the moment since I only tested it on the KL25 'till now).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Mar 2014 19:26:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K64F120-can-not-be-connected/m-p/295262#M12103</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-03-13T19:26:00Z</dc:date>
    </item>
  </channel>
</rss>