<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: SD card 4 bit mode</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SD-card-4-bit-mode/m-p/294840#M12032</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Jennie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the D4D graphic library of freescale and in some screens I need to load some pictures from SD card.&lt;/P&gt;&lt;P&gt;The operation is very slow and I'd like to improve this speed.&lt;/P&gt;&lt;P&gt;I disconnected some pins of SD card case to verify if it works in 1 bit mode or 4 bit mode and the result is: it works in 1 bit mode.&lt;/P&gt;&lt;P&gt;I think to improve the working speed it should work in 4 bit mode. How I can force it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please note that I have not experience on SD cards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you help me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Stefano&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Oct 2015 06:52:35 GMT</pubDate>
    <dc:creator>chobin</dc:creator>
    <dc:date>2015-10-07T06:52:35Z</dc:date>
    <item>
      <title>SD card 4 bit mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SD-card-4-bit-mode/m-p/294838#M12030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm developing an application software for kinetis K20. This application copeis pictures from a USB key to a SD card (class 4).&lt;/P&gt;&lt;P&gt;The final result is very slow, so I decided to enable the SD card 4 bit mode to improve the transfer speed. I tried to do it, but the application doesn't work when it writes a data block.&lt;/P&gt;&lt;P&gt;Please note that the SD code has been generated by processor expert version 10.2.&lt;/P&gt;&lt;P&gt;Does someone activated the 4 bit mode interface of SD card using a kinetis microcontroller? Does it work correctly? &lt;/P&gt;&lt;P&gt;Thank you in advance for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Mar 2014 21:26:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SD-card-4-bit-mode/m-p/294838#M12030</guid>
      <dc:creator>chobin</dc:creator>
      <dc:date>2014-03-12T21:26:07Z</dc:date>
    </item>
    <item>
      <title>Re: SD card 4 bit mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SD-card-4-bit-mode/m-p/294839#M12031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To investigate your problem correctly and efficiently, please provide us the follows:&lt;/P&gt;&lt;P&gt;1.&amp;nbsp;&amp;nbsp;&amp;nbsp; your CW version: Start the IDE and click on Help | About CodeWarrior Development Studio. Send me the version and build id.&lt;/P&gt;&lt;P&gt;2.&amp;nbsp;&amp;nbsp;&amp;nbsp; send the entire sample code folder(include .project, prm,c...) in zip format to me. so that i can test it on my side directly.&lt;/P&gt;&lt;P&gt;3.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; error screenshot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Apr 2014 10:05:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SD-card-4-bit-mode/m-p/294839#M12031</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2014-04-18T10:05:14Z</dc:date>
    </item>
    <item>
      <title>Re: SD card 4 bit mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SD-card-4-bit-mode/m-p/294840#M12032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Jennie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the D4D graphic library of freescale and in some screens I need to load some pictures from SD card.&lt;/P&gt;&lt;P&gt;The operation is very slow and I'd like to improve this speed.&lt;/P&gt;&lt;P&gt;I disconnected some pins of SD card case to verify if it works in 1 bit mode or 4 bit mode and the result is: it works in 1 bit mode.&lt;/P&gt;&lt;P&gt;I think to improve the working speed it should work in 4 bit mode. How I can force it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please note that I have not experience on SD cards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you help me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Stefano&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Oct 2015 06:52:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SD-card-4-bit-mode/m-p/294840#M12032</guid>
      <dc:creator>chobin</dc:creator>
      <dc:date>2015-10-07T06:52:35Z</dc:date>
    </item>
  </channel>
</rss>