<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Problem with Solution advisor and K21 / K22</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-with-Solution-advisor-and-K21-K22/m-p/294343#M11983</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"Pin muxing support" in solution advisor is a feature to describe if you could get or not the pin muxing options as excel file from this tool.&lt;/P&gt;&lt;P&gt;You can use K21 and K22 and chose between different pin options as are described on datasheet and reference manual for both.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a nice day,&lt;BR /&gt;Perla Moncada&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 May 2014 18:42:44 GMT</pubDate>
    <dc:creator>perlam_i_au</dc:creator>
    <dc:date>2014-05-09T18:42:44Z</dc:date>
    <item>
      <title>Problem with Solution advisor and K21 / K22</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-with-Solution-advisor-and-K21-K22/m-p/294342#M11982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm a bit confused using solution advisor with K2x series microcontrollers. It reports that K21/K22 do not support pin muxing. This excludes these microcontrollers and keeps only K20 in the possible solutions when you select more complicate peripheral set(for example when you select FlexBus + SDHC, 3 x UART , 2 x SPI &amp;amp; other peripherals).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But due to reference manuals K21/K22 in 144+ pin package supports pin muxing, so normally they has the same functionality like K20.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it a problem in solution advisor, reference manual error or I'm wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 May 2014 14:27:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-with-Solution-advisor-and-K21-K22/m-p/294342#M11982</guid>
      <dc:creator>tsvetanmudrov</dc:creator>
      <dc:date>2014-05-09T14:27:38Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with Solution advisor and K21 / K22</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-with-Solution-advisor-and-K21-K22/m-p/294343#M11983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"Pin muxing support" in solution advisor is a feature to describe if you could get or not the pin muxing options as excel file from this tool.&lt;/P&gt;&lt;P&gt;You can use K21 and K22 and chose between different pin options as are described on datasheet and reference manual for both.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a nice day,&lt;BR /&gt;Perla Moncada&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 May 2014 18:42:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-with-Solution-advisor-and-K21-K22/m-p/294343#M11983</guid>
      <dc:creator>perlam_i_au</dc:creator>
      <dc:date>2014-05-09T18:42:44Z</dc:date>
    </item>
  </channel>
</rss>