<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Interrupt latency time (cycles) in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-latency-time-cycles/m-p/293299#M11900</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looking at the Kinetis K documentation, it looks to me that you will need to do the following to reduce interrupt latency as much as possible:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Move the NVIC interrupt table to SRAM_L so that you will never incur a flash wait&lt;/LI&gt;&lt;LI&gt;Also move your interrupt handler(s) to SRAM_L&lt;BR /&gt;You will probably want to split the handling into the low latency part in ram, and do the rest from flash.&lt;/LI&gt;&lt;LI&gt;Keep your stack, and data needed for the interrupt handler in SRAM_U&lt;/LI&gt;&lt;LI&gt;Configure the crossbar switch for lowest latency for the hardware used by your handler(s).&lt;BR /&gt;For example, allow arbitration on undefined burst lengths, and park the peripheral bridge slave ports on the core system bus&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would also help to change your code to:&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_14006681804559859" jivemacro_uid="_14006681804559859" modifiedtitle="true"&gt;
&lt;P&gt;void PORTE_INT_HANDLER (void)&lt;/P&gt;
&lt;P&gt;{&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // write directly to PSOR/PCOR instead of changing PDOR&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOA_PSOR = 0x00020000;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // ISFR is w1c, so just write the bits we want to clear&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTE_ISFR = 0x01;&lt;/P&gt;
&lt;P&gt;&lt;SPAN style="font-size: 9pt; line-height: 12pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOA_PCOR = 0x00020000;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;}&lt;/P&gt;
&lt;/PRE&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_14006680220338726" jivemacro_uid="_14006680220338726" modifiedtitle="true"&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 May 2014 11:22:52 GMT</pubDate>
    <dc:creator>Laartoor</dc:creator>
    <dc:date>2014-05-21T11:22:52Z</dc:date>
    <item>
      <title>Interrupt latency time (cycles)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-latency-time-cycles/m-p/293293#M11894</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all &lt;BR /&gt;I'm checking the interrupt latency time of MK60DX256ZVLQ10.&lt;/P&gt;&lt;P&gt;The KQRUG is reporting:&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;"The NVIC is a standard module on the ARM Cortex M series. This module is closely&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;integrated with the core and provides a very low latency for entering an interrupt service&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;routine ISR (12 cycles) and exiting an ISR (12 cycles)."&lt;/P&gt;&lt;P&gt;But, I'm observing a different behaviour. It is possible to check the wave below:&lt;/P&gt;&lt;P&gt;TRACE 1: the edge that generaete the interrupt&amp;nbsp; (port E pin 0)&lt;/P&gt;&lt;P&gt;TRACE 2: a pin asserted immediately when ISR is started and deasserted at the end of ISR (port A pin 17)&lt;/P&gt;&lt;P&gt;TRACE 3: the TRACE_CLKOUT pin with system clock/2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="000.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40156iA2A5C09D1EF8767D/image-size/large?v=v2&amp;amp;px=999" role="button" title="000.png" alt="000.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is my simple ISR:&lt;/P&gt;&lt;P&gt;void PORTE_INT_HANDLER (void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;PORTE_ISFR |= 0x01;&lt;/P&gt;&lt;P&gt;GPIOA_PDOR |= 0x00020000;&lt;/P&gt;&lt;P&gt;GPIOA_PDOR &amp;amp;= ~0x00020000;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;Can someone tell me why the latency is too big than 12 cycles?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you all..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Sep 2013 14:59:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-latency-time-cycles/m-p/293293#M11894</guid>
      <dc:creator>FabioPacio</dc:creator>
      <dc:date>2013-09-06T14:59:11Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt latency time (cycles)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-latency-time-cycles/m-p/293294#M11895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the last trace, the signal you see is the core clk which is the maximum speed while the NVIC module runs at the bus clk frequency [half the core speed], This is the reason you are observing 24 clk cycles between the interruption trigger and the interruption response.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Sep 2013 16:59:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-latency-time-cycles/m-p/293294#M11895</guid>
      <dc:creator>perlam_i_au</dc:creator>
      <dc:date>2013-09-06T16:59:08Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt latency time (cycles)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-latency-time-cycles/m-p/293295#M11896</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Andrea,&lt;/P&gt;&lt;P&gt;the last trace is the TRACE_CLKOUT, it is the half of clock source. As you can see here.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Immagine.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/39989iC2897621512F380C/image-size/large?v=v2&amp;amp;px=999" role="button" title="Immagine.png" alt="Immagine.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;And the NVIC run at System clock not at Bus clock...&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Immagine2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40101iC1B77A5347CBE9A2/image-size/large?v=v2&amp;amp;px=999" role="button" title="Immagine2.png" alt="Immagine2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is someone that can help me to undertand why the latency is too big than 12 cycles?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Sep 2013 07:29:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-latency-time-cycles/m-p/293295#M11896</guid>
      <dc:creator>FabioPacio</dc:creator>
      <dc:date>2013-09-09T07:29:03Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt latency time (cycles)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-latency-time-cycles/m-p/293296#M11897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Fabio, your test is not measuring the interrupt latency. It is measuring the time from the application of the interrupt to the GPIO going high. You are forgetting to count the cycles generated by the entry overhead of the C ISR function and subsequent C bit setting statements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There will be cycles used in the set up of the C interrupt function frame. There are at least 3 cycles used for PORTE_ISFR |= 0x01. One cycle to read PortE_ISFR to a register,&amp;nbsp; one cycle to OR 0x01 into the register and a write of the register to PortE_ISFR. There are at least three cycles consumed in the setting of the output&amp;nbsp; PIN. Notice how many cycles it takes for the signal to go from high to low with back to back C GPIO write statements in your example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need to look at the assembly code of the Interrupt function to find out how many cycles are being consumed before you set the GPIO pin. You need to subtract the cycles the C function used to get an accurate read of interrupt latency.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Norm&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Sep 2013 15:59:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-latency-time-cycles/m-p/293296#M11897</guid>
      <dc:creator>ndavies</dc:creator>
      <dc:date>2013-09-09T15:59:27Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt latency time (cycles)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-latency-time-cycles/m-p/293297#M11898</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt; thank you for the clarification, but i'm not underdtandig what is appening:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; The instruction if ISR are:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0x00000000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTE_INT_HANDLER:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; cycles&lt;/P&gt;&lt;P&gt;0x00000000&amp;nbsp; 0x01A0F24D&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; movw&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r1,#53408&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&lt;/P&gt;&lt;P&gt;0x00000004&amp;nbsp; 0x0104F2C4&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; movt&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r1,#16388&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&lt;/P&gt;&lt;P&gt;0x00000008&amp;nbsp; 0x6808&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ldr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r0,[r1,#0]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2&lt;/P&gt;&lt;P&gt;0x0000000A&amp;nbsp; 0x0001F040&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; orr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r0,r0,#1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&lt;/P&gt;&lt;P&gt;0x0000000E&amp;nbsp; 0x6008&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; str&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r0,[r1,#0]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2&lt;/P&gt;&lt;P&gt;0x00000010&amp;nbsp; 0x010CF24F&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; movw&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r1,#61452&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&lt;/P&gt;&lt;P&gt;0x00000014&amp;nbsp; 0x010FF2C4&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; movt&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r1,#16399&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&lt;/P&gt;&lt;P&gt;0x00000018 0x6808&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ldr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r0,[r1,#0]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2&lt;/P&gt;&lt;P&gt;0x0000001A&amp;nbsp; 0x3000F440&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; orr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r0,r0,#131072&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&lt;/P&gt;&lt;P&gt;0x0000001E&amp;nbsp; 0x6008&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; str&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r0,[r1,#0]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; tot= 14&lt;/P&gt;&lt;P&gt;0x00000020&amp;nbsp; 0x010CF24F&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; movw&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r1,#61452&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;0x00000024&amp;nbsp; 0x010FF2C4&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; movt&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r1,#16399&lt;/P&gt;&lt;P&gt;0x00000028&amp;nbsp; 0x6808&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ldr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r0,[r1,#0]&lt;/P&gt;&lt;P&gt;0x0000002A&amp;nbsp; 0x3000F440&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; orr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r0,r0,#131072&lt;/P&gt;&lt;P&gt;0x0000002E&amp;nbsp; 0x6008&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; str&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r0,[r1,#0]&lt;/P&gt;&lt;P&gt;0x00000030&amp;nbsp; 0x4770&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; bx&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; lr&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And if these calculations are right:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SYSTEM CLOCK 96,0E+6Hz&amp;nbsp;&amp;nbsp;&amp;nbsp; --&amp;gt; T_CYCLE 10,4E-9 Sec&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;DELAYS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CYCLES&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TIME (sec)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;INTERRUPT LATECY&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 12&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; --&amp;gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 125,0E-9&lt;/P&gt;&lt;P&gt;ISR INSTRUCTIONS EXECUTION&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 14&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; --&amp;gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 145,8E-9&lt;/P&gt;&lt;P&gt;FLASH WAIT STATE@24MHz&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 41,7E-9&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; TOTAL 312,5E-9&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Why I'm measuring a delay of 420ns instead of 312?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Calibri','sans-serif'; font-size: 11pt; mso-fareast-font-family: SimSun; mso-fareast-theme-font: minor-fareast; mso-bidi-font-family: 'Times New Roman'; mso-ansi-language: IT; mso-fareast-language: ZH-CN; mso-bidi-language: AR-SA;"&gt;&lt;BR /&gt; &lt;span class="lia-inline-image-display-wrapper" image-alt="scope1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40377i3D0AB1ECCCB26DD0/image-size/large?v=v2&amp;amp;px=999" role="button" title="scope1.png" alt="scope1.png" /&gt;&lt;/span&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;OL style="list-style-type: upper-alpha;"&gt;&lt;LI&gt;CH1 --&amp;gt; PTE0&amp;nbsp; interrupt enabled on falling edge.&lt;/LI&gt;&lt;LI&gt;CH3 --&amp;gt; PTA17 toggle of pin done inside the ISR&lt;/LI&gt;&lt;LI&gt;CH4 --&amp;gt; TRACE_CLKOUT &lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Where is my mistake? can someone help me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Fabio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Sep 2013 11:52:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-latency-time-cycles/m-p/293297#M11898</guid>
      <dc:creator>FabioPacio</dc:creator>
      <dc:date>2013-09-19T11:52:36Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt latency time (cycles)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-latency-time-cycles/m-p/293298#M11899</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Fabio,&lt;/P&gt;&lt;P&gt;When you are counting clock cycles in your code sequence you are only considering the time the core takes to execute the instruction.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the MCU a write to a GPIO register traverses a Cross-bar switch and then a bus gasket and then it gets to the peripheral.&amp;nbsp; If you assume best case being the core is not in contention on the crossbar for the GPIO slave bus( a good guess in this case) then the number of cycles through the cross bar is 1-2 cycles. &lt;/P&gt;&lt;P&gt;The number of clock cycles through the peripheral gasket into the peripheral is another 1-2 cycles.&amp;nbsp; After the write completes in the core the actual write to the register could be 4 plus cycles later.&amp;nbsp; The entire operation is going to take not 2 cycles but 6 cycles. &lt;/P&gt;&lt;P&gt;If you do a read from a peripheral the core is stalled for the 2-4 cycles while the read comes back with the result.&amp;nbsp; Core execution may need to wait longer if the peripheral is in a different power domain.&amp;nbsp; Peripherals like the LLWU, LPTMR, RTC, CMP, TSI are in a seperate power domain and syncronization between domains add addition cycles. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So that is why you are measuring 420 ns actually instead of the theoretical of 312.&amp;nbsp; Because the theoretical is no accounting for the amount of time the core is waiting on the MCU read and writes to complete to the peripherals.&amp;nbsp; The serialization of events in an embedded system is complicated by the inconsistency of the timing in the MCU.&amp;nbsp; Add more complication if the core is not the only master on the cross-bar.&amp;nbsp; The DMA could be enabled and could be arbitrating for the slave bus on the cross-bar, increasing the time the core is stalled awaiting the bus to be freed from the DMA. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Philip &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Sep 2013 22:36:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-latency-time-cycles/m-p/293298#M11899</guid>
      <dc:creator>philip_drake</dc:creator>
      <dc:date>2013-09-20T22:36:17Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt latency time (cycles)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-latency-time-cycles/m-p/293299#M11900</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looking at the Kinetis K documentation, it looks to me that you will need to do the following to reduce interrupt latency as much as possible:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Move the NVIC interrupt table to SRAM_L so that you will never incur a flash wait&lt;/LI&gt;&lt;LI&gt;Also move your interrupt handler(s) to SRAM_L&lt;BR /&gt;You will probably want to split the handling into the low latency part in ram, and do the rest from flash.&lt;/LI&gt;&lt;LI&gt;Keep your stack, and data needed for the interrupt handler in SRAM_U&lt;/LI&gt;&lt;LI&gt;Configure the crossbar switch for lowest latency for the hardware used by your handler(s).&lt;BR /&gt;For example, allow arbitration on undefined burst lengths, and park the peripheral bridge slave ports on the core system bus&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would also help to change your code to:&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_14006681804559859" jivemacro_uid="_14006681804559859" modifiedtitle="true"&gt;
&lt;P&gt;void PORTE_INT_HANDLER (void)&lt;/P&gt;
&lt;P&gt;{&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // write directly to PSOR/PCOR instead of changing PDOR&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOA_PSOR = 0x00020000;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // ISFR is w1c, so just write the bits we want to clear&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTE_ISFR = 0x01;&lt;/P&gt;
&lt;P&gt;&lt;SPAN style="font-size: 9pt; line-height: 12pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOA_PCOR = 0x00020000;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;}&lt;/P&gt;
&lt;/PRE&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_14006680220338726" jivemacro_uid="_14006680220338726" modifiedtitle="true"&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 May 2014 11:22:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-latency-time-cycles/m-p/293299#M11900</guid>
      <dc:creator>Laartoor</dc:creator>
      <dc:date>2014-05-21T11:22:52Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt latency time (cycles)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-latency-time-cycles/m-p/293300#M11901</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Philip&lt;/P&gt;&lt;P&gt;I'm trying to understand how to count cycles for ARM cortex M0+ processors to be able to predict the exact behavior. I would be happy for any comment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using FRDM-KL25Z board and Kinetis Studio. &lt;/P&gt;&lt;P&gt;I have a code is like this:&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;STRONG style="color: #7f0055; font-size: 10.0pt; font-family: Consolas;"&gt;int&lt;/STRONG&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt; &lt;STRONG&gt;main&lt;/STRONG&gt;(&lt;/SPAN&gt;&lt;STRONG style="color: #7f0055; font-size: 10.0pt; font-family: Consolas;"&gt;void&lt;/STRONG&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;)&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;{&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: #3f7f5f;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; */&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SIM_SCGC5 |=0x400;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: #3f7f5f;"&gt;//enable clock to port B&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTB_PCR19 = 0x100; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: #3f7f5f;"&gt;//Make PTB19 as GPIO&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOB_PDDR|=0x80000; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: #3f7f5f;"&gt;//Make BTB19 as output pin&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;STRONG style="color: #7f0055; font-size: 10.0pt; font-family: Consolas;"&gt;while&lt;/STRONG&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;(1)&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN style="background: lightgrey;"&gt;GPIOB_PDOR&lt;/SPAN&gt; &amp;amp;= ~0x80000;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: #3f7f5f;"&gt;//turn green led on&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN style="background: lightgrey;"&gt;GPIOB_PDOR&lt;/SPAN&gt; |= 0x80000;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt; &lt;STRONG style="color: #7f0055; font-size: 10.0pt; font-family: Consolas;"&gt;return&lt;/STRONG&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt; 0;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: Consolas; color: black;"&gt;}&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Which compiles to (just the while loop):&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt;while(1)&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOB_PDOR &amp;amp;= ~0x80000; //turn green led on &amp;lt;Baldur: set pin low&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 548:&amp;nbsp;&amp;nbsp; 4b09 ldr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r3, [pc, #36]&amp;nbsp;&amp;nbsp; ; (570 &amp;lt;main+0x54&amp;gt;)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;Baldur: 2 cycles&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 54a:&amp;nbsp;&amp;nbsp; 4a09 ldr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r2, [pc, #36]&amp;nbsp;&amp;nbsp; ; (570 &amp;lt;main+0x54&amp;gt;)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;Baldur: 2 cycles&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 54c:&amp;nbsp;&amp;nbsp; 6811 ldr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r1, [r2, #0]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;Baldur: 2 cycles&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 54e:&amp;nbsp;&amp;nbsp; 4a09 ldr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r2, [pc, #36]&amp;nbsp;&amp;nbsp; ; (574 &amp;lt;main+0x58&amp;gt;)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;Baldur: 2 cycles&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 550:&amp;nbsp;&amp;nbsp; 400a ands&amp;nbsp;&amp;nbsp;&amp;nbsp; r2, r1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;Baldur: 1 cycle&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 552:&amp;nbsp;&amp;nbsp; 601a str&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r2, [r3, #0]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;Baldur: 2 cycles&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt;C:\Users\baldurtho\workspace.kds\TestProject_005\Debug/../Sources/main.c:87 (discriminator 1) &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOB_PDOR |= 0x80000;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 554:&amp;nbsp;&amp;nbsp; 4b06 ldr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r3, [pc, #24]&amp;nbsp;&amp;nbsp; ; (570 &amp;lt;main+0x54&amp;gt;)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;Baldur: 2 cycles&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 556:&amp;nbsp;&amp;nbsp; 4a06 ldr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r2, [pc, #24]&amp;nbsp;&amp;nbsp; ; (570 &amp;lt;main+0x54&amp;gt;)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;Baldur: 2 cycles&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 558:&amp;nbsp;&amp;nbsp; 6812 ldr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r2, [r2, #0]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;Baldur: 2 cycles&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 55a:&amp;nbsp;&amp;nbsp; 2180 movs&amp;nbsp;&amp;nbsp;&amp;nbsp; r1, #128&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ; 0x80&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;Baldur: 1 cycle&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 55c:&amp;nbsp;&amp;nbsp; 0309 lsls&amp;nbsp;&amp;nbsp;&amp;nbsp; r1, r1, #12&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;Baldur: 1 cycle1&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 55e:&amp;nbsp;&amp;nbsp; 430a orrs&amp;nbsp;&amp;nbsp;&amp;nbsp; r2, r1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;Baldur: 1 cycle&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 560:&amp;nbsp;&amp;nbsp; 601a str&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r2, [r3, #0]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;Baldur: 2 cycles&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt;C:\Users\baldurtho\workspace.kds\TestProject_005\Debug/../Sources/main.c:90 (discriminator 1) &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 562:&amp;nbsp;&amp;nbsp; e7f1 b.n&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 548 &amp;lt;main+0x2c&amp;gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;Baldur: 3 cycles&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 564:&amp;nbsp;&amp;nbsp; 40047000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word&amp;nbsp;&amp;nbsp; 0x40047000&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 568:&amp;nbsp;&amp;nbsp; 00001038&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word&amp;nbsp;&amp;nbsp; 0x00001038&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 56c:&amp;nbsp;&amp;nbsp; 4004a000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word&amp;nbsp;&amp;nbsp; 0x4004a000&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 570:&amp;nbsp;&amp;nbsp; 400ff040&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word&amp;nbsp;&amp;nbsp; 0x400ff040&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8.0pt; font-family: Consolas;"&gt; 574:&amp;nbsp;&amp;nbsp; fff7ffff&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .word&amp;nbsp;&amp;nbsp; 0xfff7ffff&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This code gave a square wave on the oscilloscope of 717 ns High and 618ns Low.&lt;/P&gt;&lt;P&gt;I counted instruction cycles and added to the above in &amp;lt;&amp;gt; brackets&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;(m0+ instruction set: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0432c/index.html" rel="nofollow"&gt;http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0432c/index.html&lt;/A&gt;&lt;SPAN&gt;)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To check my clock period I added 10 „nop“s and found it to be about 47.7ns. &lt;/P&gt;&lt;P&gt;So from the code without nops the 717ns is equavilent to 15 cycles and 618 is equavilent to 13 cycles&lt;/P&gt;&lt;P&gt;Low period: Counting cycles from line 552 (pin set low) to line 560 (pin set high) í count (my comments in the&amp;nbsp; &amp;lt;&amp;gt; prackets) 11 cycles when scope said 13.&lt;/P&gt;&lt;P&gt;High period: counting cycles from line 560 to&amp;nbsp; 552 i find 14 cycles but scope says 15&lt;/P&gt;&lt;P&gt;I have read that the m0+ processor has a 2 stage pipeline. Due to it I thought maybe the four 2 cycle instructions in row at line 548 to 54e would actually execute on every cycle and thus my actual program would be faster than the cycles for each instruction. But what I experience is the opposite, my code is slower than predicted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did some experiments and found that putting in one "&lt;SPAN style="font-family: Consolas; font-size: 10.6667px;"&gt;ldr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r3, [pc, #36]&lt;/SPAN&gt;" instruction (inline assembly) to the c-code prolonged the time by time comparable to two cycles and adding two "&lt;SPAN style="font-family: Consolas; font-size: 10.6667px;"&gt;ldr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r3, [pc, #36]&lt;/SPAN&gt;" in a row added four cycles. Could it be that the cycle count is given taking into account the two stage pipeline and expecting linear execution?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Freescale Kinetis processors are said to have no wait states so that should not cause the slow down.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was not able to test the length of all the instructions on my assembly output due to a strange problem: when I put in to my c-code the following: "__asm("orrs r2,r1"); I got the message that this instruction was not supported in Thumb16 mode - but I can see the instruction in my assembly above???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I saw your post I realized that the time difference from my cycle counting to the output measured could be due to bus access. Do you think that could be the case here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Again, I would be very happy for any comment.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Baldur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Nov 2015 11:36:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-latency-time-cycles/m-p/293300#M11901</guid>
      <dc:creator>baldurthorgilss</dc:creator>
      <dc:date>2015-11-19T11:36:21Z</dc:date>
    </item>
  </channel>
</rss>