<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: eGUI in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/eGUI/m-p/292850#M11827</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ali,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've been trying to do something similar. I need to change the focus state between 2 different buttons in order to change their colors according to some timer. However, whenever I call the D4D_FocusSet function or I use your code, the system goes to a halt and doesn't work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have all my buttons and schemes defined as INRAM but it isn´t working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you help me with this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Elisa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Jan 2016 14:23:10 GMT</pubDate>
    <dc:creator>elisamejia</dc:creator>
    <dc:date>2016-01-12T14:23:10Z</dc:date>
    <item>
      <title>eGUI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/eGUI/m-p/292848#M11825</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i'm doing an application from scratch on egui.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have 3 icons and i would like to navigate sequentially on them with 3 buttons (LEFT, OK, RIGHT).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;today, i'm able to catch button events (LEFT, OK, RIGHT) but impossible to change the focus to redirect event to the 2 others.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;D4D_OBJECT_F_TABSTOP option is correctly set in the ICON declaration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;D4D_FocusSet(screen,object) seems to don't work &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;do you please have an example where you are succesfully navigating between objects ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Etienne&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Jun 2013 13:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/eGUI/m-p/292848#M11825</guid>
      <dc:creator>Etienne</dc:creator>
      <dc:date>2013-06-16T13:47:54Z</dc:date>
    </item>
    <item>
      <title>Re: eGUI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/eGUI/m-p/292849#M11826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Etienne,&lt;/P&gt;&lt;P&gt;I developed an example using the on-board switches in the TWR-K70, this project was developed in CW 10.3 and using MQX 4.0.&lt;/P&gt;&lt;P&gt;I based most of the example on the thread discussion:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-message-small" data-containerid="2016" data-containertype="14" data-objectid="93504" data-objecttype="2" href="https://community.freescale.com/message/93504#93504"&gt;https://community.freescale.com/message/93504#93504&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SW1 is used to navigate between two text buttons and SW2 is used as the ENTER button.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Use the attached example as reference I am pretty sure you will find useful for you application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;-Alí&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2013 17:32:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/eGUI/m-p/292849#M11826</guid>
      <dc:creator>Ali_Pina</dc:creator>
      <dc:date>2013-08-12T17:32:02Z</dc:date>
    </item>
    <item>
      <title>Re: eGUI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/eGUI/m-p/292850#M11827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ali,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've been trying to do something similar. I need to change the focus state between 2 different buttons in order to change their colors according to some timer. However, whenever I call the D4D_FocusSet function or I use your code, the system goes to a halt and doesn't work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have all my buttons and schemes defined as INRAM but it isn´t working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you help me with this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Elisa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jan 2016 14:23:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/eGUI/m-p/292850#M11827</guid>
      <dc:creator>elisamejia</dc:creator>
      <dc:date>2016-01-12T14:23:10Z</dc:date>
    </item>
  </channel>
</rss>