<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックVBAT and 32.76kHz oscillator doubt</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VBAT-and-32-76kHz-oscillator-doubt/m-p/170224#M1181</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't understand why while the TWR-K20D50 board is powered by USB (J36 is open) and no battery is inserted, the demo program works only if J35 is closed.&lt;/P&gt;&lt;P&gt;From the datasheet of the microcontoller I have understood that Vbat powers only the RTC clock but the test on the evaluation board shows the opposite: is Vbat necessary for the system (and not only for the RTC module) in order to work properly?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What about the 32.768kHz crystal? Is it necessary if I don't want to power the RTC oscillator and if a 8MHz resonator feeds the system clock?&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Nov 2012 15:45:10 GMT</pubDate>
    <dc:creator>gabrielemarocco</dc:creator>
    <dc:date>2012-11-09T15:45:10Z</dc:date>
    <item>
      <title>VBAT and 32.76kHz oscillator doubt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VBAT-and-32-76kHz-oscillator-doubt/m-p/170224#M1181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't understand why while the TWR-K20D50 board is powered by USB (J36 is open) and no battery is inserted, the demo program works only if J35 is closed.&lt;/P&gt;&lt;P&gt;From the datasheet of the microcontoller I have understood that Vbat powers only the RTC clock but the test on the evaluation board shows the opposite: is Vbat necessary for the system (and not only for the RTC module) in order to work properly?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What about the 32.768kHz crystal? Is it necessary if I don't want to power the RTC oscillator and if a 8MHz resonator feeds the system clock?&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Nov 2012 15:45:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/VBAT-and-32-76kHz-oscillator-doubt/m-p/170224#M1181</guid>
      <dc:creator>gabrielemarocco</dc:creator>
      <dc:date>2012-11-09T15:45:10Z</dc:date>
    </item>
    <item>
      <title>Re: VBAT and 32.76kHz oscillator doubt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VBAT-and-32-76kHz-oscillator-doubt/m-p/170225#M1182</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Gabriele,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; K20D50 does not require VBAT to operate and you can use only the 8MHz crystal/resonator when RTC is not used,&amp;nbsp; but TWR-K20D50M Demo software is using the RTC module,&amp;nbsp; and any attempt to access an RTC registers&amp;nbsp; when VBAT is powered down,&amp;nbsp; will result in a bus error and causing the MCU to reset.&amp;nbsp; If you have a terminal connected to the TWR-K20D50M you will see this message when VBAT is disconnected ****default_isr entered on vector 3*****.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="JA" style="font-family: TimesLTStd-Roman; font-size: 14pt;"&gt;&lt;SPAN lang="JA" style="font-family: TimesLTStd-Roman; font-size: 14pt;"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Nov 2012 19:35:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/VBAT-and-32-76kHz-oscillator-doubt/m-p/170225#M1182</guid>
      <dc:creator>luispuebla</dc:creator>
      <dc:date>2012-11-09T19:35:38Z</dc:date>
    </item>
  </channel>
</rss>