<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 write protection set, cannot erase</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/write-protection-set-cannot-erase/m-p/292501#M11768</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, when I try to program KL05 kit in Keil, it says Erase failed(no matter if full erase or sections erase). I know that FSEC byte is 0xFE so Mass Erase is enabled and it is unsecured. The problematic firmware which stays in flash had set the write protection to first 8 kB of flash. Also, there was a Program longword command at 0x409 in which it went to Hardfault IRQ. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can debug that firmware and see the memory conent, so I know that FSEC byte is ok and first 8 kB are write protected.&lt;/P&gt;&lt;P&gt;But Keil doesnt ask me to mass erase, so how can I do it manually? Or is there any possiblity to save that kit?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ivan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Sep 2013 19:21:43 GMT</pubDate>
    <dc:creator>ivanrusnacko</dc:creator>
    <dc:date>2013-09-05T19:21:43Z</dc:date>
    <item>
      <title>write protection set, cannot erase</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/write-protection-set-cannot-erase/m-p/292501#M11768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, when I try to program KL05 kit in Keil, it says Erase failed(no matter if full erase or sections erase). I know that FSEC byte is 0xFE so Mass Erase is enabled and it is unsecured. The problematic firmware which stays in flash had set the write protection to first 8 kB of flash. Also, there was a Program longword command at 0x409 in which it went to Hardfault IRQ. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can debug that firmware and see the memory conent, so I know that FSEC byte is ok and first 8 kB are write protected.&lt;/P&gt;&lt;P&gt;But Keil doesnt ask me to mass erase, so how can I do it manually? Or is there any possiblity to save that kit?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ivan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Sep 2013 19:21:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/write-protection-set-cannot-erase/m-p/292501#M11768</guid>
      <dc:creator>ivanrusnacko</dc:creator>
      <dc:date>2013-09-05T19:21:43Z</dc:date>
    </item>
    <item>
      <title>Re: write protection set, cannot erase</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/write-protection-set-cannot-erase/m-p/292502#M11769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ivan,&lt;/P&gt;&lt;P&gt;I'm not familiar with keil, Why you don't try doing a mass erase with CW?&lt;/P&gt;&lt;P&gt;Here's a tutorial about how to do it. &lt;A href="http://mcuoneclipse.com/2012/05/28/device-is-secure/" title="http://mcuoneclipse.com/2012/05/28/device-is-secure/"&gt;Device is secure? | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Sep 2013 15:12:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/write-protection-set-cannot-erase/m-p/292502#M11769</guid>
      <dc:creator>albertovargas</dc:creator>
      <dc:date>2013-09-06T15:12:40Z</dc:date>
    </item>
  </channel>
</rss>