<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Using FRDM-KL05 board as external debugger</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FRDM-KL05-board-as-external-debugger/m-p/292418#M11760</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Erich&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 22 Jun 2013 10:47:06 GMT</pubDate>
    <dc:creator>pgo</dc:creator>
    <dc:date>2013-06-22T10:47:06Z</dc:date>
    <item>
      <title>Using FRDM-KL05 board as external debugger</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FRDM-KL05-board-as-external-debugger/m-p/292416#M11758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've used the other FRDM boards as external debuggers using USBDM but I have found what I believe is an error on the &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KL05Z"&gt;FRDMKL05 board&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the other FRDM boards there is a normally-closed jumper that isolates the SWCLK signal between the on-board chip and the 10-pin SWD connector while leaving the SWCLK connected between the K20 debugger chip and the 10-pin SWD connector.&amp;nbsp; This allows the connection of an external target for debugging.&lt;/P&gt;&lt;P&gt;The corresponding jumper on the FRDL-KL05 completely isolates the 10-pin connector and I cannot see an purpose for this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there something I'm missing?&lt;/P&gt;&lt;P&gt;Is this likely to be changed in future revisions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The jumper in question is J6 on the FRDM-KL05 schematic:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/soft_dev_tools/hardware_tools/schematics/FRDM-KL05Z_SCH.pdf?fpsp=1" title="http://cache.freescale.com/files/soft_dev_tools/hardware_tools/schematics/FRDM-KL05Z_SCH.pdf?fpsp=1"&gt;http://cache.freescale.com/files/soft_dev_tools/hardware_tools/schematics/FRDM-KL05Z_SCH.pdf?fpsp=1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Jun 2013 08:29:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FRDM-KL05-board-as-external-debugger/m-p/292416#M11758</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2013-06-15T08:29:17Z</dc:date>
    </item>
    <item>
      <title>Re: Using FRDM-KL05 board as external debugger</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FRDM-KL05-board-as-external-debugger/m-p/292417#M11759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi pgo,&lt;/P&gt;&lt;P&gt;yes, this is a known bug.&lt;/P&gt;&lt;P&gt;See &lt;A href="http://mcuoneclipse.com/2013/04/27/debug-external-processors-with-usbdm-and-freedom-board/" title="http://mcuoneclipse.com/2013/04/27/debug-external-processors-with-usbdm-and-freedom-board/"&gt;Debug External Processors with USBDM and Freedom Board | MCU on Eclipse&lt;/A&gt; which has the hardware fix for it described.&lt;/P&gt;&lt;P&gt;I have reported this schematic error to Freescale, and the wanted to have it fixed in a next board revision. I have not seen such a new board revision yet. Until then, the above workaround needs to be applied.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Jun 2013 10:26:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FRDM-KL05-board-as-external-debugger/m-p/292417#M11759</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2013-06-15T10:26:10Z</dc:date>
    </item>
    <item>
      <title>Re: Using FRDM-KL05 board as external debugger</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FRDM-KL05-board-as-external-debugger/m-p/292418#M11760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Erich&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 22 Jun 2013 10:47:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-FRDM-KL05-board-as-external-debugger/m-p/292418#M11760</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2013-06-22T10:47:06Z</dc:date>
    </item>
  </channel>
</rss>