<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックUSB voltage regulator problem</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-voltage-regulator-problem/m-p/292403#M11755</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;IN a custom design using the Kinetis K61 we have a directly connected USB interface (no ULPI), running in full-speed mode as a usb device, not host. It has protection diodes commonly used for a usb device connection on the D+ and D- lines. While testing our usb stack we connect and reconnect the cable multiple times. During this process we have managed to kill the interface on two boards in just a few days. The internal regulator seems to be shot as it only produces about a half volt from the 5V supplied. Static precautions are taken. The device descriptors are set to bus powered mode, no current requested.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has this problem been seen before?&amp;nbsp; What can we do to fix and/or prevent this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Mar 2013 14:48:04 GMT</pubDate>
    <dc:creator>jimclay</dc:creator>
    <dc:date>2013-03-12T14:48:04Z</dc:date>
    <item>
      <title>USB voltage regulator problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-voltage-regulator-problem/m-p/292403#M11755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;IN a custom design using the Kinetis K61 we have a directly connected USB interface (no ULPI), running in full-speed mode as a usb device, not host. It has protection diodes commonly used for a usb device connection on the D+ and D- lines. While testing our usb stack we connect and reconnect the cable multiple times. During this process we have managed to kill the interface on two boards in just a few days. The internal regulator seems to be shot as it only produces about a half volt from the 5V supplied. Static precautions are taken. The device descriptors are set to bus powered mode, no current requested.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has this problem been seen before?&amp;nbsp; What can we do to fix and/or prevent this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Mar 2013 14:48:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-voltage-regulator-problem/m-p/292403#M11755</guid>
      <dc:creator>jimclay</dc:creator>
      <dc:date>2013-03-12T14:48:04Z</dc:date>
    </item>
    <item>
      <title>Re: USB voltage regulator problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-voltage-regulator-problem/m-p/292404#M11756</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Hello Jim,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;Did you add series ferrites on VBUS and GDN pins from USB port? You could refer to the USB connection of a Freescale Board (Freedom) which is also Bus powered; on this board, the GND and VBUS signals from USB port are connected to ferrites, but they have internal resistance of 330 ohm. You can review these details on Freedom´s schematic, available at the following link:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;A href="http://www.freescale.com/files/soft_dev_tools/hardware_tools/schematics/FRDM-KL25Z_SCH.pdf"&gt;www.freescale.com/files/soft_dev_tools/hardware_tools/schematics/FRDM-KL25Z_SCH.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;Hope this information will be useful for you.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Calibri','sans-serif'; font-size: 11pt; mso-ansi-language: EN-US; mso-fareast-font-family: Batang; mso-bidi-font-family: 'Times New Roman'; mso-fareast-language: EN-US; mso-bidi-language: AR-SA;"&gt;Best regards! &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Calibri','sans-serif'; font-size: 11pt; mso-ansi-language: EN-US; mso-fareast-font-family: Batang; mso-bidi-font-family: 'Times New Roman'; mso-fareast-language: EN-US; mso-bidi-language: AR-SA;"&gt;/Carlos&lt;/SPAN&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Mar 2013 02:35:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-voltage-regulator-problem/m-p/292404#M11756</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2013-03-23T02:35:02Z</dc:date>
    </item>
    <item>
      <title>Re: USB voltage regulator problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-voltage-regulator-problem/m-p/292405#M11757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, we did not have the series ferrites.&amp;nbsp; Thanks for the tip.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Mar 2013 13:59:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-voltage-regulator-problem/m-p/292405#M11757</guid>
      <dc:creator>jimclay</dc:creator>
      <dc:date>2013-03-25T13:59:13Z</dc:date>
    </item>
  </channel>
</rss>