<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Help: Is it possible to use the internal load capacitor in all oscillator modes?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-Is-it-possible-to-use-the-internal-load-capacitor-in-all/m-p/292129#M11745</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, the internal load capacitors are available in all oscillator modes, only the internal feedback resistor disabled in all the modes except low power mode, so if the crystal only requires a 18pF load capacitor, internal capacitor should be enough, external capacitor is needed when the required load capacitors are greater than 30 pF.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Jun 2013 07:20:00 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2013-06-17T07:20:00Z</dc:date>
    <item>
      <title>Help: Is it possible to use the internal load capacitor in all oscillator modes?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-Is-it-possible-to-use-the-internal-load-capacitor-in-all/m-p/292128#M11744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to use the&amp;nbsp; internal load capacitor in all oscillator modes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to use the internal load capacitor in all oscillator modes or are they disabled in all modes except&amp;nbsp; "Low-frequency (32 kHz), low-power"?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reference manual says:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;When using low-frequency, low-power mode, the only external component is the&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;crystal or ceramic resonator itself. In the other oscillator modes, load capacitors (Cx, Cy)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;and feedback resistor (RF) &lt;STRONG&gt;are required&lt;/STRONG&gt;.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the crystal requires a 18pF load capacitor. Can't I use the internal load capacitor? It goes all the way from 0pF to 30pF.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jun 2013 09:16:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-Is-it-possible-to-use-the-internal-load-capacitor-in-all/m-p/292128#M11744</guid>
      <dc:creator>markosiponen</dc:creator>
      <dc:date>2013-06-14T09:16:20Z</dc:date>
    </item>
    <item>
      <title>Re: Help: Is it possible to use the internal load capacitor in all oscillator modes?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-Is-it-possible-to-use-the-internal-load-capacitor-in-all/m-p/292129#M11745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, the internal load capacitors are available in all oscillator modes, only the internal feedback resistor disabled in all the modes except low power mode, so if the crystal only requires a 18pF load capacitor, internal capacitor should be enough, external capacitor is needed when the required load capacitors are greater than 30 pF.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jun 2013 07:20:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-Is-it-possible-to-use-the-internal-load-capacitor-in-all/m-p/292129#M11745</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2013-06-17T07:20:00Z</dc:date>
    </item>
  </channel>
</rss>