<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Using DM3 as a single ended ADC input on K60 ..?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-DM3-as-a-single-ended-ADC-input-on-K60/m-p/291195#M11668</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, I've read, re-read and re-re-read the ..very.. confusing documentation for the Kinetis K60P144M120 ADC. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems to me that you can use the DM3 / DM0 pin input as a single ended input, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Given you set ADC SC1[n] ADCH to %11010.. (and that you have PGA0 up?), you should get DM0/DM3.. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the data sheet ADCH = %11010 shows a note that it is DM0 - interlaced with DM3. How do I specifically select DM0 or DM3..?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone? Am I missing something? Help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Jun 2013 17:42:02 GMT</pubDate>
    <dc:creator>toddzielinski</dc:creator>
    <dc:date>2013-06-13T17:42:02Z</dc:date>
    <item>
      <title>Using DM3 as a single ended ADC input on K60 ..?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-DM3-as-a-single-ended-ADC-input-on-K60/m-p/291195#M11668</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, I've read, re-read and re-re-read the ..very.. confusing documentation for the Kinetis K60P144M120 ADC. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems to me that you can use the DM3 / DM0 pin input as a single ended input, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Given you set ADC SC1[n] ADCH to %11010.. (and that you have PGA0 up?), you should get DM0/DM3.. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the data sheet ADCH = %11010 shows a note that it is DM0 - interlaced with DM3. How do I specifically select DM0 or DM3..?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone? Am I missing something? Help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2013 17:42:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-DM3-as-a-single-ended-ADC-input-on-K60/m-p/291195#M11668</guid>
      <dc:creator>toddzielinski</dc:creator>
      <dc:date>2013-06-13T17:42:02Z</dc:date>
    </item>
    <item>
      <title>Re: Using DM3 as a single ended ADC input on K60 ..?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-DM3-as-a-single-ended-ADC-input-on-K60/m-p/291196#M11669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This should help you understand what the "interleaved" means:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4568.pdf?fpsp=1" title="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4568.pdf?fpsp=1"&gt;http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4568.pdf?fpsp=1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For every ADC it only matters what you set in ADCH and whether you use differential measurement or not.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jun 2013 07:00:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-DM3-as-a-single-ended-ADC-input-on-K60/m-p/291196#M11669</guid>
      <dc:creator>paulmartin</dc:creator>
      <dc:date>2013-06-14T07:00:15Z</dc:date>
    </item>
  </channel>
</rss>