<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollersのトピックcannot get flashx drivers working</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/cannot-get-flashx-drivers-working/m-p/290150#M11518</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i'm devoloping a simple gui on k70 tower, using mqx 4.0.1 and egui 3 in codewarrior 10.3.&lt;/P&gt;&lt;P&gt;After an usuccesfully attemp with external nand flash, i'm trying with internal flash, using provided flashx drivers, to store some data.&lt;/P&gt;&lt;P&gt;I started from the demo, that works good, but it writes and read olny once.&lt;/P&gt;&lt;P&gt;Modifying the demo to make sequential writes and reads at the same memory address (e.g. seeking -4096 from the end), some times it misses a write, and reads the value written at the previous cycle, though write() function returns the actual size of bytes that had to be written. Some times it misses even more than 1 cycle. I can't recognize if it is a write or read issue.&lt;/P&gt;&lt;P&gt;This in ideal condition... if i change memory location (seek to), or change the length of data to be written (these are the only changes i made: seek to different location or the number of bytes to write/read), i get different erroneous behavior: such as never write, or read the correct value (the last written) only after a reset, or other erratics...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;driver problem, hw problem...? ideas?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Jun 2013 10:50:56 GMT</pubDate>
    <dc:creator>lorenzofornari</dc:creator>
    <dc:date>2013-06-13T10:50:56Z</dc:date>
    <item>
      <title>cannot get flashx drivers working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/cannot-get-flashx-drivers-working/m-p/290150#M11518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i'm devoloping a simple gui on k70 tower, using mqx 4.0.1 and egui 3 in codewarrior 10.3.&lt;/P&gt;&lt;P&gt;After an usuccesfully attemp with external nand flash, i'm trying with internal flash, using provided flashx drivers, to store some data.&lt;/P&gt;&lt;P&gt;I started from the demo, that works good, but it writes and read olny once.&lt;/P&gt;&lt;P&gt;Modifying the demo to make sequential writes and reads at the same memory address (e.g. seeking -4096 from the end), some times it misses a write, and reads the value written at the previous cycle, though write() function returns the actual size of bytes that had to be written. Some times it misses even more than 1 cycle. I can't recognize if it is a write or read issue.&lt;/P&gt;&lt;P&gt;This in ideal condition... if i change memory location (seek to), or change the length of data to be written (these are the only changes i made: seek to different location or the number of bytes to write/read), i get different erroneous behavior: such as never write, or read the correct value (the last written) only after a reset, or other erratics...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;driver problem, hw problem...? ideas?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2013 10:50:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/cannot-get-flashx-drivers-working/m-p/290150#M11518</guid>
      <dc:creator>lorenzofornari</dc:creator>
      <dc:date>2013-06-13T10:50:56Z</dc:date>
    </item>
  </channel>
</rss>