<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic K70F120M evaluation test fail, I2C0_SCL clock pin low signal problem in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70F120M-evaluation-test-fail-I2C0-SCL-clock-pin-low-signal/m-p/289745#M11486</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm evaluating I2C function for my I2C slave device.&amp;nbsp; &lt;/P&gt;&lt;P&gt;And I've failed to run it from default MXQ 3.8,1 both included I2C example and on board accel sensor quick start demo &lt;/P&gt;&lt;P&gt;(TWR-K70F120M_QSD). As well as my 0x10(7 bit address) slave device. &lt;/P&gt;&lt;P&gt;All test have stuck in the first default I2C0 poll address write:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; fwrite (xxx,xxx,..) API that go to "C:\Program Files\Freescale\Freescale MQX 3.8\mqx\source\io\i2c\polled\i2c_pol_ki2c.c"&lt;/P&gt;&lt;P&gt;line 639:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And further checked K70 board general I/O port&amp;nbsp; J5, pin3 (I2C0_SCL) by multi-meter. &lt;/P&gt;&lt;P&gt;There is only 0.11V low voltage that is different to 3.3 V working voltage required.&lt;/P&gt;&lt;P&gt;Also, double checked user_config.h I2C0 is enabled.&lt;/P&gt;&lt;P&gt;It has showed no response from the peer slave device.&lt;/P&gt;&lt;P&gt;Is it a configuration problem or a hardware de-function problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define BSPCFG_ENABLE_I2C0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&lt;/P&gt;&lt;P&gt;#define BSPCFG_ENABLE_II2C0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i2c_pol_ki2c.c:&lt;/P&gt;&lt;P&gt;uint_32 _ki2c_polled_tx(...)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; while (0 == (i2c_ptr-&amp;gt;S &amp;amp; I2C_S_IICIF_MASK))&lt;/P&gt;&lt;P&gt;... &lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 10 Mar 2013 07:20:06 GMT</pubDate>
    <dc:creator>chientsai</dc:creator>
    <dc:date>2013-03-10T07:20:06Z</dc:date>
    <item>
      <title>K70F120M evaluation test fail, I2C0_SCL clock pin low signal problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70F120M-evaluation-test-fail-I2C0-SCL-clock-pin-low-signal/m-p/289745#M11486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm evaluating I2C function for my I2C slave device.&amp;nbsp; &lt;/P&gt;&lt;P&gt;And I've failed to run it from default MXQ 3.8,1 both included I2C example and on board accel sensor quick start demo &lt;/P&gt;&lt;P&gt;(TWR-K70F120M_QSD). As well as my 0x10(7 bit address) slave device. &lt;/P&gt;&lt;P&gt;All test have stuck in the first default I2C0 poll address write:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; fwrite (xxx,xxx,..) API that go to "C:\Program Files\Freescale\Freescale MQX 3.8\mqx\source\io\i2c\polled\i2c_pol_ki2c.c"&lt;/P&gt;&lt;P&gt;line 639:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And further checked K70 board general I/O port&amp;nbsp; J5, pin3 (I2C0_SCL) by multi-meter. &lt;/P&gt;&lt;P&gt;There is only 0.11V low voltage that is different to 3.3 V working voltage required.&lt;/P&gt;&lt;P&gt;Also, double checked user_config.h I2C0 is enabled.&lt;/P&gt;&lt;P&gt;It has showed no response from the peer slave device.&lt;/P&gt;&lt;P&gt;Is it a configuration problem or a hardware de-function problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define BSPCFG_ENABLE_I2C0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&lt;/P&gt;&lt;P&gt;#define BSPCFG_ENABLE_II2C0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i2c_pol_ki2c.c:&lt;/P&gt;&lt;P&gt;uint_32 _ki2c_polled_tx(...)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; while (0 == (i2c_ptr-&amp;gt;S &amp;amp; I2C_S_IICIF_MASK))&lt;/P&gt;&lt;P&gt;... &lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 10 Mar 2013 07:20:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70F120M-evaluation-test-fail-I2C0-SCL-clock-pin-low-signal/m-p/289745#M11486</guid>
      <dc:creator>chientsai</dc:creator>
      <dc:date>2013-03-10T07:20:06Z</dc:date>
    </item>
    <item>
      <title>Re: K70F120M evaluation test fail, I2C0_SCL clock pin low signal problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70F120M-evaluation-test-fail-I2C0-SCL-clock-pin-low-signal/m-p/289746#M11487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi C&lt;SPAN class="replyToName" style="font-style: inherit; font-family: inherit;"&gt;hientsai&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you tried enabling only one of the drivers for I2C? Based of your code you are enabling interrupts and polling. Try only one of them, perhaps polling first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Vicente&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Mar 2013 18:37:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70F120M-evaluation-test-fail-I2C0-SCL-clock-pin-low-signal/m-p/289746#M11487</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2013-03-22T18:37:56Z</dc:date>
    </item>
    <item>
      <title>Re: K70F120M evaluation test fail, I2C0_SCL clock pin low signal problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70F120M-evaluation-test-fail-I2C0-SCL-clock-pin-low-signal/m-p/289747#M11488</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Chientsai!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Was this suggestion helpful? We'd like to know! :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Apr 2013 17:45:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70F120M-evaluation-test-fail-I2C0-SCL-clock-pin-low-signal/m-p/289747#M11488</guid>
      <dc:creator>Monica</dc:creator>
      <dc:date>2013-04-02T17:45:48Z</dc:date>
    </item>
  </channel>
</rss>