<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Need USB Mass Storage on FRDM-KL25Z Platform</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-USB-Mass-Storage-on-FRDM-KL25Z-Platform/m-p/288682#M11367</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The second option - no hosting and no OS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The cited example seems completely broken, but it could be something I'm doing wrong - do you have a Freedom board to try it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Feb 2014 16:01:21 GMT</pubDate>
    <dc:creator>nicknax</dc:creator>
    <dc:date>2014-02-11T16:01:21Z</dc:date>
    <item>
      <title>Need USB Mass Storage on FRDM-KL25Z Platform</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-USB-Mass-Storage-on-FRDM-KL25Z-Platform/m-p/288680#M11365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm looking for a &lt;STRONG&gt;working&lt;/STRONG&gt; example of an USB MSD on the FRDM-KL25Z platform, using CW for MCU v 10.5 and Freescale USB Stack 4.1.1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The bundled example below compiles, but a block write to the device returns a success code (# of bytes written) while subsequent readbacks show that the contents remain unmodified.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:\Freescale\Freescale USB Stack v4.1.1\ProcessorExpert\Examples\Device\MSD\USB_MSD_DEVICE_MKL25Z128_PEx\.cproject&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think the example is a bit suspect because it only creates a 1024-byte (2x 512 byte block) disk.&amp;nbsp; I've tried larger RAM sizes, but the original problem of "pretending to write" remains.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Feb 2014 22:51:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-USB-Mass-Storage-on-FRDM-KL25Z-Platform/m-p/288680#M11365</guid>
      <dc:creator>nicknax</dc:creator>
      <dc:date>2014-02-10T22:51:17Z</dc:date>
    </item>
    <item>
      <title>Re: Need USB Mass Storage on FRDM-KL25Z Platform</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-USB-Mass-Storage-on-FRDM-KL25Z-Platform/m-p/288681#M11366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Nick&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you requiring host (eg. connecting a memoery stick to the board) or device mode (looking like a disk drive to a PC)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If a device, what storage medium are you using/going to use? I would expect that this will need at least a few kbytes of disk space for the PC to be able to do anything with it (for boot sector, FAT and cluster space), so maybe the example (with very little space) is not designed to do more that show the enumeration(?). {Often an SD card would be added via SPI for decent file system space}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Feb 2014 14:30:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-USB-Mass-Storage-on-FRDM-KL25Z-Platform/m-p/288681#M11366</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-02-11T14:30:45Z</dc:date>
    </item>
    <item>
      <title>Re: Need USB Mass Storage on FRDM-KL25Z Platform</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-USB-Mass-Storage-on-FRDM-KL25Z-Platform/m-p/288682#M11367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The second option - no hosting and no OS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The cited example seems completely broken, but it could be something I'm doing wrong - do you have a Freedom board to try it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Feb 2014 16:01:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-USB-Mass-Storage-on-FRDM-KL25Z-Platform/m-p/288682#M11367</guid>
      <dc:creator>nicknax</dc:creator>
      <dc:date>2014-02-11T16:01:21Z</dc:date>
    </item>
    <item>
      <title>Re: Need USB Mass Storage on FRDM-KL25Z Platform</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-USB-Mass-Storage-on-FRDM-KL25Z-Platform/m-p/288683#M11368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Nick&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I have a feedom board. At the moment I still don't see the use of USB-MSD device without enough memory to operate a FAT in unless the FAT is being emulated (as performed by boot loaders).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I haven't used the USB Stack 4.1.1 but instead the uTasker USB stack - there is a USB-MSD loader for the freedom boards at &lt;A href="http://www.utasker.com/SW_Demos.html#KL20" title="http://www.utasker.com/SW_Demos.html#KL20"&gt;µTasker Test Software and Demos&lt;/A&gt; in case that could help checking that your board operates correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Feb 2014 16:57:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-USB-Mass-Storage-on-FRDM-KL25Z-Platform/m-p/288683#M11368</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-02-11T16:57:27Z</dc:date>
    </item>
    <item>
      <title>Re: Need USB Mass Storage on FRDM-KL25Z Platform</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-USB-Mass-Storage-on-FRDM-KL25Z-Platform/m-p/288684#M11369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the example, however, I would like to stay with the bare-metal example provided in the USB Stack 4.1.1 bundle.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I filed a technical service request a week ago, but the support tech just says "But I am sure that the original MSD USB Stack examples work fine".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I gues that's all I'm asking is if anyone can confirm that indeed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:\Freescale\Freescale USB Stack v4.1.1\ProcessorExpert\Examples\Device\MSD\USB_MSD_DEVICE_MKL25Z128_PEx\.cproject&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"works fine" on a FRDM-KL25Z board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2014 23:30:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-USB-Mass-Storage-on-FRDM-KL25Z-Platform/m-p/288684#M11369</guid>
      <dc:creator>nicknax</dc:creator>
      <dc:date>2014-02-13T23:30:48Z</dc:date>
    </item>
    <item>
      <title>Re: Need USB Mass Storage on FRDM-KL25Z Platform</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-USB-Mass-Storage-on-FRDM-KL25Z-Platform/m-p/288685#M11370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Nick&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It sounds as though you have received the answer already from the people who know ;-)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2014 23:47:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-USB-Mass-Storage-on-FRDM-KL25Z-Platform/m-p/288685#M11370</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-02-13T23:47:33Z</dc:date>
    </item>
  </channel>
</rss>