<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックDefault clock frequency for KL25 in CodeWarrior</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-clock-frequency-for-KL25-in-CodeWarrior/m-p/288386#M11299</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have started using FRDM-KL25 boards on an undergrad lab course, and in this course we use CodeWarrior 10.4, but we do not use Processor Expert. I would like to know the default clock mode and frequency that a bare metal, non-PE project configures into the KL25 microcontroller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Sep 2013 11:36:16 GMT</pubDate>
    <dc:creator>quevedo</dc:creator>
    <dc:date>2013-09-03T11:36:16Z</dc:date>
    <item>
      <title>Default clock frequency for KL25 in CodeWarrior</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-clock-frequency-for-KL25-in-CodeWarrior/m-p/288386#M11299</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have started using FRDM-KL25 boards on an undergrad lab course, and in this course we use CodeWarrior 10.4, but we do not use Processor Expert. I would like to know the default clock mode and frequency that a bare metal, non-PE project configures into the KL25 microcontroller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Sep 2013 11:36:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-clock-frequency-for-KL25-in-CodeWarrior/m-p/288386#M11299</guid>
      <dc:creator>quevedo</dc:creator>
      <dc:date>2013-09-03T11:36:16Z</dc:date>
    </item>
    <item>
      <title>Re: Default clock frequency for KL25 in CodeWarrior</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-clock-frequency-for-KL25-in-CodeWarrior/m-p/288387#M11300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On reset, the mcu uses the slow internal reference clock until you configure something else.&amp;nbsp; That's 32 kHz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Sep 2013 12:43:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-clock-frequency-for-KL25-in-CodeWarrior/m-p/288387#M11300</guid>
      <dc:creator>rogerfl</dc:creator>
      <dc:date>2013-09-03T12:43:41Z</dc:date>
    </item>
    <item>
      <title>Re: Default clock frequency for KL25 in CodeWarrior</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-clock-frequency-for-KL25-in-CodeWarrior/m-p/288388#M11301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have verified the default reset values for the registers of the MCG module. According to that, after reset it enters FEI mode, using the 32kHz internal reference, multiplied by FLL by a factor of 640, which leads to 20.48MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I still have one thing to verify. I do not know if the default startup code added by CodeWarrior in a non-PE project modifies any of the default parameters, changing clock frequency. My bet is that the startup code does not handle hardware too much, so it must keep default values. I think I will program a TPM channel to output compare and check the output frequency, relating it with the internal system clock.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Sep 2013 13:15:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-clock-frequency-for-KL25-in-CodeWarrior/m-p/288388#M11301</guid>
      <dc:creator>quevedo</dc:creator>
      <dc:date>2013-09-03T13:15:31Z</dc:date>
    </item>
    <item>
      <title>Re: Default clock frequency for KL25 in CodeWarrior</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-clock-frequency-for-KL25-in-CodeWarrior/m-p/288389#M11302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Antonio&lt;/P&gt;&lt;P&gt;if you're using your FRDM-KL25 boards with the settings used by defaul the internal oscillator 32KHz FLL.. The frequency defaul is of 20.9MHZ.&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Important to see that setup is if (FEI ENgaged Internal clock mode) or (FBI Bypassed Internal clock mode). you can check this:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38361i8F363421A1BB1E41/image-size/large?v=v2&amp;amp;px=999" title="MCG.png" alt="MCG.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Sep 2013 14:08:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-clock-frequency-for-KL25-in-CodeWarrior/m-p/288389#M11302</guid>
      <dc:creator>emmanuelballest</dc:creator>
      <dc:date>2013-09-03T14:08:53Z</dc:date>
    </item>
    <item>
      <title>Re: Default clock frequency for KL25 in CodeWarrior</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-clock-frequency-for-KL25-in-CodeWarrior/m-p/288390#M11303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I finally got it! I have done a test using a timer to toggle an output pin, and connected my logic analyser to this pin, measuring high and low times. I have programmed the timer prescaler to divide by 128, which would give us a timer clock frequency of 160kHz, if original system clock is the expected 20.84MHz. Using a timer module of 160, I should have one toggle every 1ms, which I confirmed in my measurements. Thus, I conclude that bare metal projects without Processor Expert, in CW10.4, for KL25 processor, keeps the default clock source: FEI mode, system frequency of 20.48MHz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Sep 2013 12:27:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-clock-frequency-for-KL25-in-CodeWarrior/m-p/288390#M11303</guid>
      <dc:creator>quevedo</dc:creator>
      <dc:date>2013-09-05T12:27:03Z</dc:date>
    </item>
    <item>
      <title>Re: Default clock frequency for KL25 in CodeWarrior</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-clock-frequency-for-KL25-in-CodeWarrior/m-p/288391#M11304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;That´s right¡ &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Sep 2013 14:23:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-clock-frequency-for-KL25-in-CodeWarrior/m-p/288391#M11304</guid>
      <dc:creator>emmanuelballest</dc:creator>
      <dc:date>2013-09-05T14:23:58Z</dc:date>
    </item>
  </channel>
</rss>