<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Kinetis K60 and ISO7816 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K60-and-ISO7816/m-p/287811#M11243</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are also looking for the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Trying to connect the KL27Z to the smart card J3D081 (&lt;A class="link-titled" href="https://www.commoncriteriaportal.org/files/epfiles/0860b_pdf.pdf" title="https://www.commoncriteriaportal.org/files/epfiles/0860b_pdf.pdf"&gt;https://www.commoncriteriaportal.org/files/epfiles/0860b_pdf.pdf&lt;/A&gt;&amp;nbsp;). Just need to send the ATR and read the response over ISO7816. We have been able to get the same working on the LPC11U24 but even after spending considerable amount of time we have made much progress.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Neel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Aug 2017 10:21:51 GMT</pubDate>
    <dc:creator>ND2</dc:creator>
    <dc:date>2017-08-23T10:21:51Z</dc:date>
    <item>
      <title>Kinetis K60 and ISO7816</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K60-and-ISO7816/m-p/287808#M11240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everyone!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to connect two Smart-Cards to K60, UART0 and UART1 support ISO7816.&lt;/P&gt;&lt;P&gt;Smart-Card ISO7816 has CLK and I/O.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I/O is to be connected to appropriate UART-TX of the MCU in accordance with Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But where am I to connect CLK of Smart-Card?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Feb 2014 13:47:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K60-and-ISO7816/m-p/287808#M11240</guid>
      <dc:creator>SergeMaslenniko</dc:creator>
      <dc:date>2014-02-10T13:47:03Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K60 and ISO7816</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K60-and-ISO7816/m-p/287809#M11241</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Serge&lt;/P&gt;&lt;P&gt;You can connect CLK to a flex timer output pin directly. &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42691iBDC2C62859572E85/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope my reply can help you. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2014 07:27:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K60-and-ISO7816/m-p/287809#M11241</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2014-02-18T07:27:39Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K60 and ISO7816</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K60-and-ISO7816/m-p/287810#M11242</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul,&lt;/P&gt;&lt;P&gt;Do we have reference design, appnote, and/or example project for Kinetis doing ISO7816 support?&lt;/P&gt;&lt;P&gt;Customer looking for K60 or K64 level of capability.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Apr 2015 18:08:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K60-and-ISO7816/m-p/287810#M11242</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2015-04-16T18:08:42Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K60 and ISO7816</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K60-and-ISO7816/m-p/287811#M11243</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are also looking for the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Trying to connect the KL27Z to the smart card J3D081 (&lt;A class="link-titled" href="https://www.commoncriteriaportal.org/files/epfiles/0860b_pdf.pdf" title="https://www.commoncriteriaportal.org/files/epfiles/0860b_pdf.pdf"&gt;https://www.commoncriteriaportal.org/files/epfiles/0860b_pdf.pdf&lt;/A&gt;&amp;nbsp;). Just need to send the ATR and read the response over ISO7816. We have been able to get the same working on the LPC11U24 but even after spending considerable amount of time we have made much progress.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Neel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Aug 2017 10:21:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K60-and-ISO7816/m-p/287811#M11243</guid>
      <dc:creator>ND2</dc:creator>
      <dc:date>2017-08-23T10:21:51Z</dc:date>
    </item>
  </channel>
</rss>