<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IAR setting for I-jet with Kinetis in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/IAR-setting-for-I-jet-with-Kinetis/m-p/287648#M11229</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello MF,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having the exact issue with the same debugger &amp;amp; IAR when using with K60 MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please let ne know how you have solved this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gopi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Jul 2014 08:06:41 GMT</pubDate>
    <dc:creator>GopiNagaBharath</dc:creator>
    <dc:date>2014-07-17T08:06:41Z</dc:date>
    <item>
      <title>IAR setting for I-jet with Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/IAR-setting-for-I-jet-with-Kinetis/m-p/287646#M11227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I wanted to share an issue using IAR and an I-Jet to program a Kinetis MCU for the first time.&amp;nbsp; In this case, it was a K70, but after working on it, the customer figured it out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the I-jet, initially they could not establish a connection with the two boards to program or debug.&amp;nbsp; The MCU was identified successfully over JTAG, but the reset sequence failed.&amp;nbsp; The JLink connected with no issue at all.&amp;nbsp; They also found that after the JLink had programmed the MCU, then they were able to re-program just fine with the I-Jet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then they played with a blank board that had not been touched yet.&amp;nbsp; And they found by changing the Reset option in IAR to Hardware, as shown below, the I-Jet was able to connect and program the blank board with no issue.&amp;nbsp; IAR had defaulted to this Reset setting to Custom.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119147iA21FF9FC124FCE22/image-size/large?v=v2&amp;amp;px=999" title="IAR.jpg" alt="IAR.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Mar 2013 20:04:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/IAR-setting-for-I-jet-with-Kinetis/m-p/287646#M11227</guid>
      <dc:creator>dereksnell</dc:creator>
      <dc:date>2013-03-07T20:04:25Z</dc:date>
    </item>
    <item>
      <title>Re: IAR setting for I-jet with Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/IAR-setting-for-I-jet-with-Kinetis/m-p/287647#M11228</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Derek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using IAR and I-jet on custum board with K40. (256KB P-Flash, 256KB Flex NVM)&lt;/P&gt;&lt;P&gt;Until this week, everything work fine: Debug mode, program the MCU, download file, erase memory and so on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This week, when we connect the I-jet to the board, the "DBG" LED in the I-jet is blinking, and we cannot communicate with the MCU. the message is: "Fatal error: CPU did not power up&amp;nbsp;&amp;nbsp; Session aborted! "&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the scope we see that the reset pin of the K40 MCU is ossilating every ~40 us. We try to change the configurations of "Reset" options in the IAR IDE, as you described, but it is not help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any idea how can we communicate with the MCU?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another thing. this failure occur after try to "play" with code examples from: "&lt;STRONG style="font-size: 11.0pt; font-family: 'Times New Roman','serif';"&gt;Standard Software Driver for C90TFS Flash"&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;MF&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Jun 2013 13:33:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/IAR-setting-for-I-jet-with-Kinetis/m-p/287647#M11228</guid>
      <dc:creator>mf_kappa</dc:creator>
      <dc:date>2013-06-30T13:33:56Z</dc:date>
    </item>
    <item>
      <title>Re: IAR setting for I-jet with Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/IAR-setting-for-I-jet-with-Kinetis/m-p/287648#M11229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello MF,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having the exact issue with the same debugger &amp;amp; IAR when using with K60 MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please let ne know how you have solved this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gopi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jul 2014 08:06:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/IAR-setting-for-I-jet-with-Kinetis/m-p/287648#M11229</guid>
      <dc:creator>GopiNagaBharath</dc:creator>
      <dc:date>2014-07-17T08:06:41Z</dc:date>
    </item>
  </channel>
</rss>