<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K40 FOR IAR in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K40-FOR-IAR/m-p/168779#M1109</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This sounds to be normal operation. GPIOC_PSOR﻿ is the&amp;nbsp;Set Output Register﻿, causing the bit with '1' to be set to the output; the register itself always reads 0.&lt;/P&gt;&lt;P&gt;Since the write set the bit in the output, this is seen in the GPIOC_PDORC﻿ register.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;By contrast, if you write "GPIOC_PCOR﻿ = 1" it will then clear the bit in the GPIOC_PDORC﻿ register.&lt;/P&gt;&lt;P&gt;Furthermore "GPIOC_PTOR﻿ = 1"﻿ will toggle the bit.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Sep 2011 06:43:43 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2011-09-23T06:43:43Z</dc:date>
    <item>
      <title>K40 FOR IAR</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K40-FOR-IAR/m-p/168778#M1108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use the IAR ARM sample example,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;when i set "GPIOC_PSOR = 1" ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;the Register will set to "GPIOC_PDORC = 1" .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2011 15:17:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K40-FOR-IAR/m-p/168778#M1108</guid>
      <dc:creator>WayneChung</dc:creator>
      <dc:date>2011-09-22T15:17:57Z</dc:date>
    </item>
    <item>
      <title>Re: K40 FOR IAR</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K40-FOR-IAR/m-p/168779#M1109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This sounds to be normal operation. GPIOC_PSOR﻿ is the&amp;nbsp;Set Output Register﻿, causing the bit with '1' to be set to the output; the register itself always reads 0.&lt;/P&gt;&lt;P&gt;Since the write set the bit in the output, this is seen in the GPIOC_PDORC﻿ register.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;By contrast, if you write "GPIOC_PCOR﻿ = 1" it will then clear the bit in the GPIOC_PDORC﻿ register.&lt;/P&gt;&lt;P&gt;Furthermore "GPIOC_PTOR﻿ = 1"﻿ will toggle the bit.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Sep 2011 06:43:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K40-FOR-IAR/m-p/168779#M1109</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2011-09-23T06:43:43Z</dc:date>
    </item>
  </channel>
</rss>