<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Can't connect. No suitable USBDM debug interface was located(ARM GDI Protocol Adapter),</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-connect-No-suitable-USBDM-debug-interface-was-located-ARM/m-p/285745#M10958</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Pgo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your reply and sharing.&lt;/P&gt;&lt;P&gt;The link is very useful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Jan 2014 03:33:07 GMT</pubDate>
    <dc:creator>nguyennhatminh</dc:creator>
    <dc:date>2014-01-07T03:33:07Z</dc:date>
    <item>
      <title>Can't connect. No suitable USBDM debug interface was located(ARM GDI Protocol Adapter),</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-connect-No-suitable-USBDM-debug-interface-was-located-ARM/m-p/285743#M10956</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a board FRDM-KL05Z, I just try to build and debug, but it doesn't work and gave me the message :" Can't connect. No suitable USBDM debug interface was located(ARM GDI Protocol Adapter)"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anyone tell me the reason ? in the connection i choose USBDM debug, and OpenSDA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think do should i buy a debugger/programmer from P&amp;amp;E such as USB Multilink Universal All-In-One Development Interface, then re-configure in Run-&amp;gt;Run configuration, and Edit connection style,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;your response will be highly appreciate.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Minh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Jan 2014 10:23:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-connect-No-suitable-USBDM-debug-interface-was-located-ARM/m-p/285743#M10956</guid>
      <dc:creator>nguyennhatminh</dc:creator>
      <dc:date>2014-01-04T10:23:59Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect. No suitable USBDM debug interface was located(ARM GDI Protocol Adapter),</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-connect-No-suitable-USBDM-debug-interface-was-located-ARM/m-p/285744#M10957</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nguyen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You have several choices for how to program the FRDM boards:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P&amp;amp;E's OpenSDA based debugger:&lt;/P&gt;&lt;P&gt;This is the one that is included standard in Freescale's software.&amp;nbsp; You can follow the quick start guide that comes with the board or download the quick start package:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/software/board_support_packages/FRDM-KL25Z_QSP.zip" title="http://cache.freescale.com/files/32bit/software/board_support_packages/FRDM-KL25Z_QSP.zip"&gt;http://cache.freescale.com/files/32bit/software/board_support_packages/FRDM-KL25Z_QSP.zip&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;USBDM&lt;/P&gt;&lt;P&gt;This is an open source interface which you need to install separately.&amp;nbsp; From the error message you provided it is likely that you have installed the USBDM software but have not installed the firmware on the board.&amp;nbsp; See if this page helps (you don't need to do the hardware changes unless you want to program an external board.&amp;nbsp; Follow the instructions from &lt;STRONG&gt;Installing USBDM firmware on FRDM-KL25Z:&lt;/STRONG&gt;&amp;nbsp; You can try the stand-alone programmers to check the board operations.&lt;/P&gt;&lt;P&gt;&lt;A href="http://usbdm.sourceforge.net/USBDM_V4.10/Freedom/html/freedom_setup.html" title="http://usbdm.sourceforge.net/USBDM_V4.10/Freedom/html/freedom_setup.html"&gt;USBDM: Setting Up the FRDM-KL25Z&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CMSIS (I haven't actually used it)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There's lots of useful information at:&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/" title="http://mcuoneclipse.com/"&gt;MCU on Eclipse | Everything on Eclipse, Microcontrollers and Software&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Jan 2014 15:19:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-connect-No-suitable-USBDM-debug-interface-was-located-ARM/m-p/285744#M10957</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2014-01-04T15:19:57Z</dc:date>
    </item>
    <item>
      <title>Re: Can't connect. No suitable USBDM debug interface was located(ARM GDI Protocol Adapter),</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-connect-No-suitable-USBDM-debug-interface-was-located-ARM/m-p/285745#M10958</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Pgo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your reply and sharing.&lt;/P&gt;&lt;P&gt;The link is very useful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jan 2014 03:33:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-connect-No-suitable-USBDM-debug-interface-was-located-ARM/m-p/285745#M10958</guid>
      <dc:creator>nguyennhatminh</dc:creator>
      <dc:date>2014-01-07T03:33:07Z</dc:date>
    </item>
  </channel>
</rss>