<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Kinetis KL26xx - USB clock (48 MHz) from 32.768 KHz crystal?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KL26xx-USB-clock-48-MHz-from-32-768-KHz-crystal/m-p/284898#M10898</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;32.768 kHz crystals are not very accurate so it would be best to use a good crystal for USB reliability..8MHz have much better accuracy.&lt;/P&gt;&lt;P&gt;For experimental purposes it is possible to control the 32kHz crystal loading a bit to tune it better but I wouldn't use such for a real product since it would probably cause more trouble that any cost savings are worth.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Mar 2014 17:01:29 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2014-03-11T17:01:29Z</dc:date>
    <item>
      <title>Kinetis KL26xx - USB clock (48 MHz) from 32.768 KHz crystal?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KL26xx-USB-clock-48-MHz-from-32-768-KHz-crystal/m-p/284897#M10897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to get fully working USB only with 32,768 KHz crystal?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am able to use FLL to get 47.972352 MHz. USB works but only with some USB host controllers. With the others USB enumeration failed with result "Unknown device". &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;If I use 8 MHz crystal with PLL to get exactly 48 MHz, USB works with all tested&amp;nbsp; USB host controllers.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tested program is the same, it only differs in clock settings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anyone who was able to operate USB with 32,768 KHz crystal?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Mar 2014 09:16:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KL26xx-USB-clock-48-MHz-from-32-768-KHz-crystal/m-p/284897#M10897</guid>
      <dc:creator>merlin69</dc:creator>
      <dc:date>2014-03-10T09:16:05Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis KL26xx - USB clock (48 MHz) from 32.768 KHz crystal?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KL26xx-USB-clock-48-MHz-from-32-768-KHz-crystal/m-p/284898#M10898</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;32.768 kHz crystals are not very accurate so it would be best to use a good crystal for USB reliability..8MHz have much better accuracy.&lt;/P&gt;&lt;P&gt;For experimental purposes it is possible to control the 32kHz crystal loading a bit to tune it better but I wouldn't use such for a real product since it would probably cause more trouble that any cost savings are worth.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Mar 2014 17:01:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KL26xx-USB-clock-48-MHz-from-32-768-KHz-crystal/m-p/284898#M10898</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-03-11T17:01:29Z</dc:date>
    </item>
  </channel>
</rss>