<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: FreeMaster</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FreeMaster/m-p/284423#M10838</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Jingjing, the example works great now!&lt;/P&gt;&lt;P&gt;It actually worked with both the PEMicro MSD bootloader, but also with the PEMicro debug app (as well as the latest integrated version 114 from PEMicro) . I guess that's because they both implement the serial pass through.&lt;/P&gt;&lt;P&gt;So I will try and use the PEMicro for debug instead of CMSIS DAP...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you briefly outline the steps needed to add this basic functionality to my application? (let's say I just want to view/edit one variable)&lt;/P&gt;&lt;P&gt;1/ do I need to make any changes to my code (I would like to use driverless mode if possible)&lt;/P&gt;&lt;P&gt;2/ how do I configure the TSA table in Freemaster?&lt;/P&gt;&lt;P&gt;3/ In the file FMSTRUG it says that there is a plugin for P&amp;amp;E BDM, however in version 1.4 I could only find 2 plugins: iSystem winIDEA, and Segger/Jlink. Has the P&amp;amp;E been deprecated in this version? Is it available in older versions? Do you know which one?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Jan 2014 18:39:04 GMT</pubDate>
    <dc:creator>andreag</dc:creator>
    <dc:date>2014-01-03T18:39:04Z</dc:date>
    <item>
      <title>FreeMaster</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FreeMaster/m-p/284421#M10836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to connect my PC with mt FRDM-KL25Z for demo purposes.&lt;/P&gt;&lt;P&gt;For development/debugging I am using Keil and CMSIS-DAP, but I want people to lay with my application with a simple interface.&lt;/P&gt;&lt;P&gt;Freemaster would seemd the perfect solution, but I am getting lost in all the options.&lt;/P&gt;&lt;P&gt;There is a posting somwehere else on this forum:&lt;A href="https://community.nxp.com/docs/DOC-95001"&gt;Touch sensing demo for Freedom KL25z for MSD bootloader&lt;/A&gt;&lt;/P&gt;&lt;P&gt;where it seems that this is possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What are the requirements though for the driverless configuration?&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Is the connection through the OpenSDA interface of the onboard USB?&lt;/LI&gt;&lt;LI&gt;can I leave CMSIS_DAP on the OpenSDA chip, or something specific is needed there?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What additional requirements for the operation with the Freemaster driver?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jan 2014 00:49:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FreeMaster/m-p/284421#M10836</guid>
      <dc:creator>andreag</dc:creator>
      <dc:date>2014-01-03T00:49:06Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMaster</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FreeMaster/m-p/284422#M10837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrea Gorgerino,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Did you can't run the posting: &lt;A _jive_internal="true" data-containerid="2019" data-containertype="14" data-objectid="95001" data-objecttype="102" href="https://community.nxp.com/docs/DOC-95001"&gt;Touch sensing demo for Freedom KL25z for MSD bootloader&lt;/A&gt; correctly?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1, you should make sure your board mode is in MSD bootloader,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; you can find this bootloader in the quick start package, please download it from this link:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KL25Z&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&amp;amp;uc=true&amp;amp;lang_cd=en" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KL25Z&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&amp;amp;uc=true&amp;amp;lang_cd=en"&gt;FRDM-KL25Z: Freescale Freedom Development Platform for Kinetis KL14/15/24/25 MCUs&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2,Actually, the connection between the FreeMaster and FRDM-KL25Z is the uart0, so you should choose the correct COM and configure the baud rate to 38400.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; you can configure it in the freemaster softe: Project-&amp;gt;options, then like the following picture:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41249iEC37DC7D4BD70E2C/image-size/large?v=v2&amp;amp;px=999" title="9.jpg" alt="9.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; you can find your com port from your computer management, like the following:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41294i20C8DDFA413BF6AB/image-size/large?v=v2&amp;amp;px=999" title="10.jpg" alt="10.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;then start the freemaster,&amp;nbsp; and touch the slide in the freedom board, you will find the freemaster scope like the following:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41232iA533F3BE5F16F497/image-size/large?v=v2&amp;amp;px=999" title="11.jpg" alt="11.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question ,please let me know~!&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;Jingjing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jan 2014 02:55:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FreeMaster/m-p/284422#M10837</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2014-01-03T02:55:17Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMaster</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FreeMaster/m-p/284423#M10838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Jingjing, the example works great now!&lt;/P&gt;&lt;P&gt;It actually worked with both the PEMicro MSD bootloader, but also with the PEMicro debug app (as well as the latest integrated version 114 from PEMicro) . I guess that's because they both implement the serial pass through.&lt;/P&gt;&lt;P&gt;So I will try and use the PEMicro for debug instead of CMSIS DAP...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you briefly outline the steps needed to add this basic functionality to my application? (let's say I just want to view/edit one variable)&lt;/P&gt;&lt;P&gt;1/ do I need to make any changes to my code (I would like to use driverless mode if possible)&lt;/P&gt;&lt;P&gt;2/ how do I configure the TSA table in Freemaster?&lt;/P&gt;&lt;P&gt;3/ In the file FMSTRUG it says that there is a plugin for P&amp;amp;E BDM, however in version 1.4 I could only find 2 plugins: iSystem winIDEA, and Segger/Jlink. Has the P&amp;amp;E been deprecated in this version? Is it available in older versions? Do you know which one?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jan 2014 18:39:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FreeMaster/m-p/284423#M10838</guid>
      <dc:creator>andreag</dc:creator>
      <dc:date>2014-01-03T18:39:04Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMaster</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FreeMaster/m-p/284424#M10839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;STRONG class="font-color-meta"&gt;&lt;SPAN class="replyToName"&gt;Andrea Gorgerino,&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to notice that &lt;SPAN class="replyToName"&gt;you can also work with remote access. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;You can invite the possibility - &lt;SPAN class="replyToName"&gt;communication between 2 computers. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;&lt;SPAN class="replyToName"&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;You can try it with HTTP or DCOM.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;Please, visit the document &lt;A href="https://community.nxp.com/docs/DOC-103293"&gt;FREEMASTER:&amp;nbsp; Remote Server Tutorial&lt;/A&gt;&lt;/SPAN&gt;&lt;STRONG class="font-color-meta"&gt;&lt;SPAN class="replyToName"&gt; &lt;BR /&gt;&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope you find it also useful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Iva&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Mar 2015 13:25:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FreeMaster/m-p/284424#M10839</guid>
      <dc:creator>ivadorazinova</dc:creator>
      <dc:date>2015-03-17T13:25:45Z</dc:date>
    </item>
  </channel>
</rss>