<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 console IO interrupt uart5</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/console-IO-interrupt-uart5/m-p/283887#M10745</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Helllo, &lt;/P&gt;&lt;P&gt;currently I am using a TWM k60 evm module. &lt;/P&gt;&lt;P&gt;I would like to use the console IO component trough UART5, and I would like to be able to enable interrupts on this component.&lt;/P&gt;&lt;P&gt;Anyway, using ProcessorExpert, I am not able to change "Interrupt/service event" value into enable because it is disabled.&lt;/P&gt;&lt;P&gt;I previously enabled CPU's NMI.&lt;/P&gt;&lt;P&gt;I suppose is "obvious" not enabling interrupts on port used as debug purpose, but I am not sure.&lt;/P&gt;&lt;P&gt;Any hint would be gladly appreciated. &lt;/P&gt;&lt;P&gt;Best regards, &lt;/P&gt;&lt;P&gt;Luca. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Feb 2014 14:51:27 GMT</pubDate>
    <dc:creator>Catosh</dc:creator>
    <dc:date>2014-02-07T14:51:27Z</dc:date>
    <item>
      <title>console IO interrupt uart5</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/console-IO-interrupt-uart5/m-p/283887#M10745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Helllo, &lt;/P&gt;&lt;P&gt;currently I am using a TWM k60 evm module. &lt;/P&gt;&lt;P&gt;I would like to use the console IO component trough UART5, and I would like to be able to enable interrupts on this component.&lt;/P&gt;&lt;P&gt;Anyway, using ProcessorExpert, I am not able to change "Interrupt/service event" value into enable because it is disabled.&lt;/P&gt;&lt;P&gt;I previously enabled CPU's NMI.&lt;/P&gt;&lt;P&gt;I suppose is "obvious" not enabling interrupts on port used as debug purpose, but I am not sure.&lt;/P&gt;&lt;P&gt;Any hint would be gladly appreciated. &lt;/P&gt;&lt;P&gt;Best regards, &lt;/P&gt;&lt;P&gt;Luca. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Feb 2014 14:51:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/console-IO-interrupt-uart5/m-p/283887#M10745</guid>
      <dc:creator>Catosh</dc:creator>
      <dc:date>2014-02-07T14:51:27Z</dc:date>
    </item>
    <item>
      <title>Re: console IO interrupt uart5</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/console-IO-interrupt-uart5/m-p/283888#M10746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Luca,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Yes, you are right, the console IO component&amp;nbsp; is really can't set the the interrupt function, because it is the integrated component.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you want to use the interruption, you can choose the "Serial_LDD" component, "AsynchroSerial" component or "Init_UART" component, these components can set the interrupts.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; You just choose wrong component.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Wish my answer will help you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you still have question, please let me know!&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;Jingjing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 Feb 2014 06:06:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/console-IO-interrupt-uart5/m-p/283888#M10746</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2014-02-08T06:06:49Z</dc:date>
    </item>
  </channel>
</rss>