<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K70 Graphical LCD controller support in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Graphical-LCD-controller-support/m-p/283506#M10707</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Pedro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply. This is really helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Dani&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Apr 2013 12:52:45 GMT</pubDate>
    <dc:creator>danif</dc:creator>
    <dc:date>2013-04-26T12:52:45Z</dc:date>
    <item>
      <title>K70 Graphical LCD controller support</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Graphical-LCD-controller-support/m-p/283504#M10705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is mentioned in the specification of K70 controller that it has Graphical LCD controller for 800x600 pixel resolution LCD. I have three questions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1 - How to run a graphical LCD with more than 800x600 resolution.&lt;/P&gt;&lt;P&gt;2 - Can K70 enter into low power modes while Graphical LCD keeps on displaying without any disturbance.&lt;/P&gt;&lt;P&gt;3 - Can a graphical LCD controller be used to run a segmented LCD..if yes how?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Dani&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Apr 2013 17:10:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Graphical-LCD-controller-support/m-p/283504#M10705</guid>
      <dc:creator>danif</dc:creator>
      <dc:date>2013-04-24T17:10:43Z</dc:date>
    </item>
    <item>
      <title>Re: K70 Graphical LCD controller support</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Graphical-LCD-controller-support/m-p/283505#M10706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1.- You can interface the LCDC module with larger displays however the controller will only send a 800x600 image, leaving the rest of the display inactive.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.- As you can see in the following table extracted from the Reference manual, the LCDC module retains full functionality in VLPR and VLPW&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119301i8B65EB130F35304E/image-size/large?v=v2&amp;amp;px=999" title="4012_4012.png" alt="4012_4012.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.- I'm afraid the K70 LCDC module can only interface with graphic displays, however you can use any of the GPIO ports to achieve segment LCD communication.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Apr 2013 17:26:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Graphical-LCD-controller-support/m-p/283505#M10706</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2013-04-25T17:26:58Z</dc:date>
    </item>
    <item>
      <title>Re: K70 Graphical LCD controller support</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Graphical-LCD-controller-support/m-p/283506#M10707</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Pedro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply. This is really helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Dani&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Apr 2013 12:52:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Graphical-LCD-controller-support/m-p/283506#M10707</guid>
      <dc:creator>danif</dc:creator>
      <dc:date>2013-04-26T12:52:45Z</dc:date>
    </item>
  </channel>
</rss>