<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollersのトピックcodewarrior debug error:No source available for &amp;quot;0x00000172&amp;quot;</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/codewarrior-debug-error-No-source-available-for-quot-0x00000172/m-p/283282#M10680</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial, Helvetica, sans-serif; font-size: 10pt;"&gt;environment:coderwarrior 10.4 &lt;BR /&gt;MCU:the MKL20 MCU &lt;BR /&gt;Burner:P&amp;amp;E micro &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial, Helvetica, sans-serif; font-size: 10pt;"&gt;I build a bareboard project.&lt;BR /&gt;When I debug will appear as &lt;BR /&gt;shown in the annex of the case. &lt;BR /&gt;It will run over with no error When I run, &lt;BR /&gt;but no code download to the Flash. &lt;BR /&gt;Please tell me ,How can I do to solve &lt;BR /&gt;this problem. &lt;BR /&gt;Thanks a lot;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 09 Jun 2013 01:56:39 GMT</pubDate>
    <dc:creator>陈欣</dc:creator>
    <dc:date>2013-06-09T01:56:39Z</dc:date>
    <item>
      <title>codewarrior debug error:No source available for "0x00000172"</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/codewarrior-debug-error-No-source-available-for-quot-0x00000172/m-p/283282#M10680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial, Helvetica, sans-serif; font-size: 10pt;"&gt;environment:coderwarrior 10.4 &lt;BR /&gt;MCU:the MKL20 MCU &lt;BR /&gt;Burner:P&amp;amp;E micro &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial, Helvetica, sans-serif; font-size: 10pt;"&gt;I build a bareboard project.&lt;BR /&gt;When I debug will appear as &lt;BR /&gt;shown in the annex of the case. &lt;BR /&gt;It will run over with no error When I run, &lt;BR /&gt;but no code download to the Flash. &lt;BR /&gt;Please tell me ,How can I do to solve &lt;BR /&gt;this problem. &lt;BR /&gt;Thanks a lot;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 09 Jun 2013 01:56:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/codewarrior-debug-error-No-source-available-for-quot-0x00000172/m-p/283282#M10680</guid>
      <dc:creator>陈欣</dc:creator>
      <dc:date>2013-06-09T01:56:39Z</dc:date>
    </item>
    <item>
      <title>Re: codewarrior debug error:No source available for "0x00000172"</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/codewarrior-debug-error-No-source-available-for-quot-0x00000172/m-p/283283#M10681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Chen Xin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For you could use CW V10.4 debug the board and CW V10.4 default debug target is FLASH targe.&amp;nbsp; I think you have program the Flas successfully before the code debug. Otherwise it could not debug the code. If after your debug the code, you couldn't run the code without debugger? You need to check the MCU VDD power up ramp rate, it need Keep instantaneous slew rate of VDD below 17 kV/sec.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 09 Jun 2013 03:10:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/codewarrior-debug-error-No-source-available-for-quot-0x00000172/m-p/283283#M10681</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2013-06-09T03:10:58Z</dc:date>
    </item>
    <item>
      <title>Re: codewarrior debug error:No source available for "0x00000172"</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/codewarrior-debug-error-No-source-available-for-quot-0x00000172/m-p/283284#M10682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chen Xin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About how to generate ".hex" image file of CW V10.4 project.&lt;/P&gt;&lt;P&gt;In CW project Properties, select [C/C++ Build] -&amp;gt; [Setting] -&amp;gt;[Additional Tools]: select [Create Flash Image]&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119478iDEB3301790CD9B00/image-size/large?v=v2&amp;amp;px=999" title="create flash image.jpg" alt="create flash image.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Then In [ARM Ltd Windows GNU Create Flash Image] select [Output file format]:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119479iBB5EA82F24856B74/image-size/large?v=v2&amp;amp;px=999" title="output file formate.jpg" alt="output file formate.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Then you can recompile the project and in [FLASH] target folder, you will find genrated ".hex" image file.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 09 Jun 2013 05:29:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/codewarrior-debug-error-No-source-available-for-quot-0x00000172/m-p/283284#M10682</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2013-06-09T05:29:19Z</dc:date>
    </item>
    <item>
      <title>Re: codewarrior debug error:No source available for "0x00000172"</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/codewarrior-debug-error-No-source-available-for-quot-0x00000172/m-p/283285#M10683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks very much!&lt;/P&gt;&lt;P&gt;&lt;SPAN class="hps"&gt;You&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;help me greatly!:smileyhappy:&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 09 Jun 2013 06:16:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/codewarrior-debug-error-No-source-available-for-quot-0x00000172/m-p/283285#M10683</guid>
      <dc:creator>陈欣</dc:creator>
      <dc:date>2013-06-09T06:16:21Z</dc:date>
    </item>
  </channel>
</rss>