<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic K10,AD question in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-AD-question/m-p/282027#M10476</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Hi,everyone,I have two questions about the AD module of kinetic.&lt;/P&gt;&lt;P&gt;1. where's the hardware trigger source ,that is ADHWTSn ? I'm wondering if it means&amp;nbsp; the IO port the AD channel is using?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; if it is,can I change the channel by just writting new channel numbers into the&amp;nbsp; ADCH while the former conversion is under hardware trigger mode.&lt;/P&gt;&lt;P&gt;2.what's the ADC A, B means ,is it just for those channels with "a" or "b" suffix ,like the ADC0 _SE4a &amp;amp;ADC0_SE4b,then how about the channels with no suffix? I mean if&amp;nbsp; I want to use the channel AD19,should I write the ADCx_SC1A or ADCx_SC1B or both?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Apr 2013 03:10:21 GMT</pubDate>
    <dc:creator>fugrace</dc:creator>
    <dc:date>2013-04-24T03:10:21Z</dc:date>
    <item>
      <title>K10,AD question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-AD-question/m-p/282027#M10476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Hi,everyone,I have two questions about the AD module of kinetic.&lt;/P&gt;&lt;P&gt;1. where's the hardware trigger source ,that is ADHWTSn ? I'm wondering if it means&amp;nbsp; the IO port the AD channel is using?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; if it is,can I change the channel by just writting new channel numbers into the&amp;nbsp; ADCH while the former conversion is under hardware trigger mode.&lt;/P&gt;&lt;P&gt;2.what's the ADC A, B means ,is it just for those channels with "a" or "b" suffix ,like the ADC0 _SE4a &amp;amp;ADC0_SE4b,then how about the channels with no suffix? I mean if&amp;nbsp; I want to use the channel AD19,should I write the ADCx_SC1A or ADCx_SC1B or both?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Apr 2013 03:10:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-AD-question/m-p/282027#M10476</guid>
      <dc:creator>fugrace</dc:creator>
      <dc:date>2013-04-24T03:10:21Z</dc:date>
    </item>
    <item>
      <title>Re: K10,AD question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-AD-question/m-p/282028#M10477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Grace&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For your question1: ADC hardware triggers are from PDB not GPIO. ADC can have more then one status and control register: one for each conversion. TheSC1B–SC1n registers indicate potentially multiple SC1 registers for use only in hardware trigger mode. Each ADC module has ADCx_SC1A and ADCx_SC1B. For each ADCx_SC1A and ADCx_SC1B has a data result register.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;For your question2: For SC1A and SC1B usage, you can reference question1 reply. This A and B is not use as ADC0 _SE4a &amp;amp;ADC0_SE4b. ADC0 _SE4a &amp;amp;ADC0_SE4b are used for flexible channel selection. If you want to use AD19, you need to write to ADCx_SC1A.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Hope my reply can help you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Best Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Paul&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Apr 2013 08:25:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-AD-question/m-p/282028#M10477</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2013-04-24T08:25:55Z</dc:date>
    </item>
    <item>
      <title>Re: K10,AD question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-AD-question/m-p/282029#M10478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much,it's very useful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Apr 2013 11:16:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-AD-question/m-p/282029#M10478</guid>
      <dc:creator>fugrace</dc:creator>
      <dc:date>2013-04-24T11:16:18Z</dc:date>
    </item>
  </channel>
</rss>