<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Kinetis K60 Bootloader &amp; JTAG reference in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K60-Bootloader-JTAG-reference/m-p/281123#M10394</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mithun,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Do you mean the bootloader via UART/USB port? if yes, please kindly refer to an2295(serial boot) &lt;A href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295.pdf?fsrch=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;sr=1"&gt;http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295.pdf &lt;/A&gt;and the demo code from &lt;A href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295SW_Rev1.zip?fsrch=1"&gt;http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295SW_Rev1.zip?fsrch=1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Or you may refer to an4370(USB DFU bootloader) from &lt;A href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4370.pdf"&gt;http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4370.pdf&lt;/A&gt; and the demo code from &lt;A href="http://www.freescale.com/webapp/sps/download/license.jsp?colCode=AN4370SW&amp;amp;location=null&amp;amp;fsrch=1&amp;amp;Parent_nodeId=from%20search&amp;amp;Parent_pageType=from%20search"&gt;http://www.freescale.com/webapp/sps/download/license.jsp?colCode=AN4370SW&amp;amp;location=null&amp;amp;fsrch=1&amp;amp;Parent_nodeId=from%20search&amp;amp;Parent_pageType=from%20search&lt;/A&gt;&lt;/P&gt;&lt;P&gt;2. You may use FTM module to capture the falling edge. There are multiple channels in one FTM module, so you need't use 4 FTM modules to do that.&lt;/P&gt;&lt;P&gt;3. do you mean the falling edge event? if so , I think also the FTM timer can be used for that purpose, but the counter clock source should use EXTCLK — FTM External Clock which connected with the IO that falling edge happens on it. alternatively, I think you may also use a GPIO interrupt which is falling edge sensitive , a variable used to store the counter which increased in the interrupt service.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Kan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Jul 2013 09:05:50 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2013-07-19T09:05:50Z</dc:date>
    <item>
      <title>Kinetis K60 Bootloader &amp; JTAG reference</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K60-Bootloader-JTAG-reference/m-p/281122#M10393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One of my customer is using&amp;nbsp; &lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;MK60FX5125VLQ12&lt;/SPAN&gt;, &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Please suggest me on the below &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. They want to use ISP (UART/USB) for field programming, please suggest how to implement this. Please also suggest which UART port is suitable to implement this, please also share if any source code available for the implementation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. They want to use 4 timers for Capturing falling edge, which timers can be used for this also let us know will these timers work concurrently.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. They need one counter for counting the events, which timer is preferred for event counting.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Mithun &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jul 2013 18:09:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K60-Bootloader-JTAG-reference/m-p/281122#M10393</guid>
      <dc:creator>mithunp_s</dc:creator>
      <dc:date>2013-07-18T18:09:47Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K60 Bootloader &amp; JTAG reference</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K60-Bootloader-JTAG-reference/m-p/281123#M10394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mithun,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Do you mean the bootloader via UART/USB port? if yes, please kindly refer to an2295(serial boot) &lt;A href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295.pdf?fsrch=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;sr=1"&gt;http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295.pdf &lt;/A&gt;and the demo code from &lt;A href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295SW_Rev1.zip?fsrch=1"&gt;http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295SW_Rev1.zip?fsrch=1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Or you may refer to an4370(USB DFU bootloader) from &lt;A href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4370.pdf"&gt;http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4370.pdf&lt;/A&gt; and the demo code from &lt;A href="http://www.freescale.com/webapp/sps/download/license.jsp?colCode=AN4370SW&amp;amp;location=null&amp;amp;fsrch=1&amp;amp;Parent_nodeId=from%20search&amp;amp;Parent_pageType=from%20search"&gt;http://www.freescale.com/webapp/sps/download/license.jsp?colCode=AN4370SW&amp;amp;location=null&amp;amp;fsrch=1&amp;amp;Parent_nodeId=from%20search&amp;amp;Parent_pageType=from%20search&lt;/A&gt;&lt;/P&gt;&lt;P&gt;2. You may use FTM module to capture the falling edge. There are multiple channels in one FTM module, so you need't use 4 FTM modules to do that.&lt;/P&gt;&lt;P&gt;3. do you mean the falling edge event? if so , I think also the FTM timer can be used for that purpose, but the counter clock source should use EXTCLK — FTM External Clock which connected with the IO that falling edge happens on it. alternatively, I think you may also use a GPIO interrupt which is falling edge sensitive , a variable used to store the counter which increased in the interrupt service.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Kan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jul 2013 09:05:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K60-Bootloader-JTAG-reference/m-p/281123#M10394</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2013-07-19T09:05:50Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K60 Bootloader &amp; JTAG reference</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K60-Bootloader-JTAG-reference/m-p/281124#M10395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the details, this information is very useful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mithun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 20 Jul 2013 03:45:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K60-Bootloader-JTAG-reference/m-p/281124#M10395</guid>
      <dc:creator>mithunp_s</dc:creator>
      <dc:date>2013-07-20T03:45:14Z</dc:date>
    </item>
  </channel>
</rss>