<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: kl04 is secured</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl04-is-secured/m-p/280834#M10338</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here are two videos, them show how to erase and unsecure devices using Code Warrior and J-Link,&lt;BR /&gt;I hope you find them useful&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a nice day :P,&lt;BR /&gt;Perla&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Mar 2014 21:01:21 GMT</pubDate>
    <dc:creator>perlam_i_au</dc:creator>
    <dc:date>2014-03-11T21:01:21Z</dc:date>
    <item>
      <title>kl04 is secured</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl04-is-secured/m-p/280833#M10337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;PRE&gt;Hello,
I am trying to program a custom board (KL04) via the Multilink.It worked fine, but then it shows the "Device is secure.Erase to unsecure".I keep pressing Yes.
AFter doing this twice the "Multilink" not connected is shown. There was another board that was doing the same.
&lt;P&gt;But, its now, surprisingly working,except this 1 board.&lt;/P&gt;
&lt;P&gt;I tried the Processor halt utility. Still no luck.Uninstalled/installed PE drivers. No luck.&lt;/P&gt;
&lt;P&gt;Also, no where in the code have I modified that register (FTFA_FOPT or any such dangerous registers:) .&lt;/P&gt;
&lt;P&gt;Infact CODE WARRIOR warns you if you make any changes to such registers.).
Also, is there any way I can ensure such a message/error does not occur in any future boards. Can this be done via s/w code or so. 
I saw in a site that I can look at the Binary files at the location 0x40C. How can I look at 0x40C. Kindly help me out. This is a disaster as 1 board is beyond recovery :smileysad:&lt;/P&gt;
&lt;/PRE&gt;&lt;PRE&gt;Vinod.&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Mar 2014 20:58:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl04-is-secured/m-p/280833#M10337</guid>
      <dc:creator>vinkar</dc:creator>
      <dc:date>2014-03-06T20:58:18Z</dc:date>
    </item>
    <item>
      <title>Re: kl04 is secured</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl04-is-secured/m-p/280834#M10338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here are two videos, them show how to erase and unsecure devices using Code Warrior and J-Link,&lt;BR /&gt;I hope you find them useful&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a nice day :P,&lt;BR /&gt;Perla&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Mar 2014 21:01:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl04-is-secured/m-p/280834#M10338</guid>
      <dc:creator>perlam_i_au</dc:creator>
      <dc:date>2014-03-11T21:01:21Z</dc:date>
    </item>
  </channel>
</rss>