<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K10DN32VFM5 clocking option</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10DN32VFM5-clocking-option/m-p/167285#M1029</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks I do not plan to use the real time clock (RTC) on the product so that will not be an issue.&lt;/P&gt;&lt;P&gt;The K10 can be clock at 50MHz using the slow IRC and the FLL as I have found in the reference manual, so at the moment I believe I should be able to use the K10 without an external clock for the proposed project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 03 Jun 2012 21:06:30 GMT</pubDate>
    <dc:creator>Dan1234</dc:creator>
    <dc:date>2012-06-03T21:06:30Z</dc:date>
    <item>
      <title>K10DN32VFM5 clocking option</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10DN32VFM5-clocking-option/m-p/167283#M1027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am planning on using the K10DN32VFM part.&lt;/P&gt;&lt;P&gt;My question is when clocking with the 32 KHz IRC through the FLL, will it be possible to generate max Core/system clock speed (50 MHz)?&lt;/P&gt;&lt;P&gt;Are there any peripherals that require an external clock to operate or will they all work with only the clock generated using the 32 KHz IRC and the FLL?&lt;/P&gt;&lt;P&gt;I have been through the data sheets and believe that I can use the IRC but just making sure I am not missing anything obvious as this is my first attempt to use an ARM on a project and the amount of data I am having to read and understand just&amp;nbsp; to chose a suitable part is quite a lot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Thanks,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 May 2012 18:34:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10DN32VFM5-clocking-option/m-p/167283#M1027</guid>
      <dc:creator>Dan1234</dc:creator>
      <dc:date>2012-05-29T18:34:30Z</dc:date>
    </item>
    <item>
      <title>Re: K10DN32VFM5 clocking option</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10DN32VFM5-clocking-option/m-p/167284#M1028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You will not be able to use RTC module with only IRC. It always requires external 32kHz crystal.&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jun 2012 15:39:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10DN32VFM5-clocking-option/m-p/167284#M1028</guid>
      <dc:creator>PetrC</dc:creator>
      <dc:date>2012-06-01T15:39:14Z</dc:date>
    </item>
    <item>
      <title>Re: K10DN32VFM5 clocking option</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10DN32VFM5-clocking-option/m-p/167285#M1029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks I do not plan to use the real time clock (RTC) on the product so that will not be an issue.&lt;/P&gt;&lt;P&gt;The K10 can be clock at 50MHz using the slow IRC and the FLL as I have found in the reference manual, so at the moment I believe I should be able to use the K10 without an external clock for the proposed project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 03 Jun 2012 21:06:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10DN32VFM5-clocking-option/m-p/167285#M1029</guid>
      <dc:creator>Dan1234</dc:creator>
      <dc:date>2012-06-03T21:06:30Z</dc:date>
    </item>
  </channel>
</rss>