<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is there a non-blocking version of FlashEraseSector()? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-there-a-non-blocking-version-of-FlashEraseSector/m-p/279035#M10152</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It seems that when you call this function, it will not return until the erase has been completed, so it could block other code from running for many hundreds of milliseconds. Is there a non-blocking version of this function that can be polled for erase completed?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Feb 2013 22:03:53 GMT</pubDate>
    <dc:creator>davidwhite</dc:creator>
    <dc:date>2013-02-28T22:03:53Z</dc:date>
    <item>
      <title>Is there a non-blocking version of FlashEraseSector()?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-there-a-non-blocking-version-of-FlashEraseSector/m-p/279035#M10152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It seems that when you call this function, it will not return until the erase has been completed, so it could block other code from running for many hundreds of milliseconds. Is there a non-blocking version of this function that can be polled for erase completed?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Feb 2013 22:03:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-there-a-non-blocking-version-of-FlashEraseSector/m-p/279035#M10152</guid>
      <dc:creator>davidwhite</dc:creator>
      <dc:date>2013-02-28T22:03:53Z</dc:date>
    </item>
    <item>
      <title>Re: Is there a non-blocking version of FlashEraseSector()?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-there-a-non-blocking-version-of-FlashEraseSector/m-p/279036#M10153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FSL recommend the use of the C90TFS_Flash drivers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;A href="http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe?fpsp=1&amp;amp;WT_TYPE=Device%20Drivers&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=exe&amp;amp;WT_ASSET=Downloads&amp;amp;sr=26" title="http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe?fpsp=1&amp;amp;WT_TYPE=Device%20Drivers&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=exe&amp;amp;WT_ASSET=Downloads&amp;amp;sr=26"&gt;http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe?fpsp=1&amp;amp;WT_TYPE=Device%20Drivers&amp;amp;WT_VENDOR=FREESC… &lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Think they should serve the purpose. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are looking to customize further you may but then make sure while erasing you are not accessing in the same block.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Mar 2013 04:17:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-there-a-non-blocking-version-of-FlashEraseSector/m-p/279036#M10153</guid>
      <dc:creator>deepakrana</dc:creator>
      <dc:date>2013-03-01T04:17:47Z</dc:date>
    </item>
  </channel>
</rss>