<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPSPI module- keeping chip select active in K32 L Series Microcontrollers</title>
    <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/LPSPI-module-keeping-chip-select-active/m-p/1467202#M84</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I'm using LPSPI module of K32L2A41VLL1A to send/receive data to/from External flash. My requirement is to first send command data with Rx buffer null and then receive the buffer with tx null. i.e., after sending command there's a second send/receive function to retrieve the received buffer. But I'm not able to get that data. Can you help me with the configurations I have to do so that the Rx buffer data is not lost during my second transaction?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;Shri&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 01 Jun 2022 05:44:23 GMT</pubDate>
    <dc:creator>SK_98</dc:creator>
    <dc:date>2022-06-01T05:44:23Z</dc:date>
    <item>
      <title>LPSPI module- keeping chip select active</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/LPSPI-module-keeping-chip-select-active/m-p/1467202#M84</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I'm using LPSPI module of K32L2A41VLL1A to send/receive data to/from External flash. My requirement is to first send command data with Rx buffer null and then receive the buffer with tx null. i.e., after sending command there's a second send/receive function to retrieve the received buffer. But I'm not able to get that data. Can you help me with the configurations I have to do so that the Rx buffer data is not lost during my second transaction?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;Shri&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Jun 2022 05:44:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/LPSPI-module-keeping-chip-select-active/m-p/1467202#M84</guid>
      <dc:creator>SK_98</dc:creator>
      <dc:date>2022-06-01T05:44:23Z</dc:date>
    </item>
    <item>
      <title>Re: LPSPI module- keeping chip select active</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/LPSPI-module-keeping-chip-select-active/m-p/1467227#M85</link>
      <description>&lt;P&gt;After send command data with Rx buffer null, lpspi pull cs high.You can Transfer with rx no null and tx no null.&lt;/P&gt;&lt;P&gt;RT1170，&lt;SPAN class=""&gt;for reference：&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="hefan_2-1654064485616.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/181894iFF087AD42FA624FF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="hefan_2-1654064485616.png" alt="hefan_2-1654064485616.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="hefan_1-1654064347837.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/181893i721BF2B95B060429/image-size/medium?v=v2&amp;amp;px=400" role="button" title="hefan_1-1654064347837.png" alt="hefan_1-1654064347837.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Jun 2022 06:22:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/LPSPI-module-keeping-chip-select-active/m-p/1467227#M85</guid>
      <dc:creator>hefan</dc:creator>
      <dc:date>2022-06-01T06:22:30Z</dc:date>
    </item>
  </channel>
</rss>