<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>K32 L Series MicrocontrollersのトピックRe: K25Z Migration to K32L2B</title>
    <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/K25Z-Migration-to-K32L2B/m-p/1444882#M73</link>
    <description>&lt;P&gt;If your application is based on MCUXpresso SDK, then migration thing will be easy.&lt;/P&gt;
&lt;P&gt;The same type peripheral driver APIs are almost the same, for example the I2C driver API is similar to LPI2C driver API&lt;/P&gt;</description>
    <pubDate>Mon, 18 Apr 2022 05:05:17 GMT</pubDate>
    <dc:creator>jay_heng</dc:creator>
    <dc:date>2022-04-18T05:05:17Z</dc:date>
    <item>
      <title>K25Z Migration to K32L2B</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/K25Z-Migration-to-K32L2B/m-p/1444230#M71</link>
      <description>&lt;P&gt;Hi folks.&lt;/P&gt;&lt;P&gt;I would like to migrate from &lt;STRONG&gt;FRDM-KL25Z&lt;/STRONG&gt; to &lt;STRONG&gt;FRDM-K32L2B3&lt;/STRONG&gt;, but I'm not sure what the differences are.&lt;/P&gt;&lt;P&gt;From what I've seen they are very similar, with some specific differences, such as: the K32L is from 2019, while the KL25Z is from 2012, the K32L's I2C driver is a little different (and more problematic), etc...&lt;/P&gt;&lt;P&gt;But what are all the changes? Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Thu, 14 Apr 2022 15:40:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/K25Z-Migration-to-K32L2B/m-p/1444230#M71</guid>
      <dc:creator>pedrobotelho15</dc:creator>
      <dc:date>2022-04-14T15:40:25Z</dc:date>
    </item>
    <item>
      <title>Re: K25Z Migration to K32L2B</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/K25Z-Migration-to-K32L2B/m-p/1444880#M72</link>
      <description>&lt;P&gt;From peripheral point of view, KL25 is quiet different from K32L. As most of KL25 peripheral registers are 8bit width while K32L peripheral registers are 32bit.&lt;/P&gt;
&lt;P&gt;So the peripheral is different, It is I2C in KL25 while LPI2C in K32L.&lt;/P&gt;
&lt;P&gt;K32L is much similar to KL03/KL43/KL27 parts.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 18 Apr 2022 05:01:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/K25Z-Migration-to-K32L2B/m-p/1444880#M72</guid>
      <dc:creator>jay_heng</dc:creator>
      <dc:date>2022-04-18T05:01:35Z</dc:date>
    </item>
    <item>
      <title>Re: K25Z Migration to K32L2B</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/K25Z-Migration-to-K32L2B/m-p/1444882#M73</link>
      <description>&lt;P&gt;If your application is based on MCUXpresso SDK, then migration thing will be easy.&lt;/P&gt;
&lt;P&gt;The same type peripheral driver APIs are almost the same, for example the I2C driver API is similar to LPI2C driver API&lt;/P&gt;</description>
      <pubDate>Mon, 18 Apr 2022 05:05:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/K25Z-Migration-to-K32L2B/m-p/1444882#M73</guid>
      <dc:creator>jay_heng</dc:creator>
      <dc:date>2022-04-18T05:05:17Z</dc:date>
    </item>
    <item>
      <title>Re: K25Z Migration to K32L2B</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/K25Z-Migration-to-K32L2B/m-p/1445108#M74</link>
      <description>&lt;P&gt;Oh, I get it. I thought all of KL25Z peripheral registers where 32-bits as well.&lt;/P&gt;</description>
      <pubDate>Mon, 18 Apr 2022 12:18:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/K25Z-Migration-to-K32L2B/m-p/1445108#M74</guid>
      <dc:creator>pedrobotelho15</dc:creator>
      <dc:date>2022-04-18T12:18:42Z</dc:date>
    </item>
    <item>
      <title>Re: K25Z Migration to K32L2B</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/K25Z-Migration-to-K32L2B/m-p/1446406#M77</link>
      <description>&lt;P&gt;App notes for the KL28 will be helpful, as the KL28 is closest to the K32L in function for LPCI2C.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Apr 2022 12:31:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/K25Z-Migration-to-K32L2B/m-p/1446406#M77</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2022-04-20T12:31:43Z</dc:date>
    </item>
  </channel>
</rss>