<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>K32 L Series MicrocontrollersのトピックK32L2B3 SWD Pin Overwrite - Debug error: 02: failed on connect could not connect to core</title>
    <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/K32L2B3-SWD-Pin-Overwrite-Debug-error-02-failed-on-connect-could/m-p/1154079#M5</link>
    <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I just started working with a Freedom Development Board for the K32L2B3 MCU series (&lt;A href="https://www.nxp.com/design/development-boards/freedom-development-boards/mcu-boards/nxp-freedom-development-platform-for-k32-l2b-mcus:FRDM-K32L2B3" target="_blank"&gt;https://www.nxp.com/design/development-boards/freedom-development-boards/mcu-boards/nxp-freedom-development-platform-for-k32-l2b-mcus:FRDM-K32L2B3&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;During some tests, the SWD(PTA3 Pin) got multiplexed as GPIO. After this, the debugger does not seem to connect properly anymore (i.e. I cannot reprogram the device). The error that I receive is: "02: failed on connect could not connect to core" as soon as I click on debug with one of the SDK example programs (these worked fine in the beginning).&lt;/P&gt;&lt;P&gt;I tried holding the reset button during the debug sequence, but this gives the error: "Cannot halt processor Failed on chip setup: Ep(04). Cannot halt processor."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any way to reset the SWD Pin functionality on the K32L2B3 series?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks.&lt;/P&gt;</description>
    <pubDate>Wed, 16 Sep 2020 09:51:36 GMT</pubDate>
    <dc:creator>JonCan</dc:creator>
    <dc:date>2020-09-16T09:51:36Z</dc:date>
    <item>
      <title>K32L2B3 SWD Pin Overwrite - Debug error: 02: failed on connect could not connect to core</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/K32L2B3-SWD-Pin-Overwrite-Debug-error-02-failed-on-connect-could/m-p/1154079#M5</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I just started working with a Freedom Development Board for the K32L2B3 MCU series (&lt;A href="https://www.nxp.com/design/development-boards/freedom-development-boards/mcu-boards/nxp-freedom-development-platform-for-k32-l2b-mcus:FRDM-K32L2B3" target="_blank"&gt;https://www.nxp.com/design/development-boards/freedom-development-boards/mcu-boards/nxp-freedom-development-platform-for-k32-l2b-mcus:FRDM-K32L2B3&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;During some tests, the SWD(PTA3 Pin) got multiplexed as GPIO. After this, the debugger does not seem to connect properly anymore (i.e. I cannot reprogram the device). The error that I receive is: "02: failed on connect could not connect to core" as soon as I click on debug with one of the SDK example programs (these worked fine in the beginning).&lt;/P&gt;&lt;P&gt;I tried holding the reset button during the debug sequence, but this gives the error: "Cannot halt processor Failed on chip setup: Ep(04). Cannot halt processor."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any way to reset the SWD Pin functionality on the K32L2B3 series?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 16 Sep 2020 09:51:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/K32L2B3-SWD-Pin-Overwrite-Debug-error-02-failed-on-connect-could/m-p/1154079#M5</guid>
      <dc:creator>JonCan</dc:creator>
      <dc:date>2020-09-16T09:51:36Z</dc:date>
    </item>
  </channel>
</rss>