<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>K32 L Series Microcontrollers中的主题 What is the clock for TSTMR?</title>
    <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/What-is-the-clock-for-TSTMR/m-p/1222827#M31</link>
    <description>&lt;P&gt;The K32 L2A Reference Manual in 50.3 states:&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN class="fontstyle0"&gt;"The TSTMR runs off the 1 MHz clock and resets on every system reset.&lt;/SPAN&gt;&amp;nbsp;"&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;What 1 MHz clock?&lt;BR /&gt;Do not see anything about it in the clock tool.&lt;BR /&gt;&lt;BR /&gt;There are a couple of vague references in the rest of the RM (Table 5-1,54-1, ) that seems to imply that the 1 MHz clock comes from SIR/8.&amp;nbsp; Nothing explains what happens to TSTMR if SIR is turned off to save power.&lt;BR /&gt;&lt;BR /&gt;?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 28 Jan 2021 19:05:34 GMT</pubDate>
    <dc:creator>bobpaddock</dc:creator>
    <dc:date>2021-01-28T19:05:34Z</dc:date>
    <item>
      <title>What is the clock for TSTMR?</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/What-is-the-clock-for-TSTMR/m-p/1222827#M31</link>
      <description>&lt;P&gt;The K32 L2A Reference Manual in 50.3 states:&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN class="fontstyle0"&gt;"The TSTMR runs off the 1 MHz clock and resets on every system reset.&lt;/SPAN&gt;&amp;nbsp;"&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;What 1 MHz clock?&lt;BR /&gt;Do not see anything about it in the clock tool.&lt;BR /&gt;&lt;BR /&gt;There are a couple of vague references in the rest of the RM (Table 5-1,54-1, ) that seems to imply that the 1 MHz clock comes from SIR/8.&amp;nbsp; Nothing explains what happens to TSTMR if SIR is turned off to save power.&lt;BR /&gt;&lt;BR /&gt;?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 28 Jan 2021 19:05:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/What-is-the-clock-for-TSTMR/m-p/1222827#M31</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2021-01-28T19:05:34Z</dc:date>
    </item>
  </channel>
</rss>