<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>K32 L Series MicrocontrollersのトピックPortE on K32L3A6</title>
    <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/PortE-on-K32L3A6/m-p/1213541#M28</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I test the FRDM-K32L3A6&amp;nbsp;&lt;/P&gt;&lt;P&gt;in the file K32L3A60_cm4.h (under the folder device) there is on line 6992 to 7000&lt;/P&gt;&lt;P&gt;definition of PORTE, but if i understand the reference manual this port is only accessible for the&amp;nbsp;&lt;/P&gt;&lt;P&gt;cortex m0+ core, so this definition can be removed ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;also in file pin_mux.h, there is&amp;nbsp;&lt;/P&gt;&lt;P&gt;void BOARD_InitPins_cm4(void); /* Function assigned for the Cortex-M4F */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;with definition for SW3 to SW5 connected to the portE, so this can be removed also.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 18 Jan 2021 17:53:21 GMT</pubDate>
    <dc:creator>darknight</dc:creator>
    <dc:date>2021-01-18T17:53:21Z</dc:date>
    <item>
      <title>PortE on K32L3A6</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/PortE-on-K32L3A6/m-p/1213541#M28</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I test the FRDM-K32L3A6&amp;nbsp;&lt;/P&gt;&lt;P&gt;in the file K32L3A60_cm4.h (under the folder device) there is on line 6992 to 7000&lt;/P&gt;&lt;P&gt;definition of PORTE, but if i understand the reference manual this port is only accessible for the&amp;nbsp;&lt;/P&gt;&lt;P&gt;cortex m0+ core, so this definition can be removed ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;also in file pin_mux.h, there is&amp;nbsp;&lt;/P&gt;&lt;P&gt;void BOARD_InitPins_cm4(void); /* Function assigned for the Cortex-M4F */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;with definition for SW3 to SW5 connected to the portE, so this can be removed also.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 18 Jan 2021 17:53:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/PortE-on-K32L3A6/m-p/1213541#M28</guid>
      <dc:creator>darknight</dc:creator>
      <dc:date>2021-01-18T17:53:21Z</dc:date>
    </item>
    <item>
      <title>Re: PortE on K32L3A6</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/PortE-on-K32L3A6/m-p/1219807#M29</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;erratum, the cortex M4 can access port E, so all is good, just a configuration is missed from the sdk :&amp;nbsp;&lt;/P&gt;&lt;P&gt;/* Clock Gate Control: Clock enabled. The current clock selection and divider options are locked. */&lt;BR /&gt;CLOCK_EnableClock(kCLOCK_Rgpio1);&lt;STRONG&gt; // this line must be add to access GPIO_BASE address&amp;nbsp;&lt;/STRONG&gt;&lt;BR /&gt;CLOCK_EnableClock(kCLOCK_PortE);&lt;STRONG&gt;// this line is generated from sdk or configtools&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks to the support.&lt;/P&gt;</description>
      <pubDate>Fri, 22 Jan 2021 18:27:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/PortE-on-K32L3A6/m-p/1219807#M29</guid>
      <dc:creator>darknight</dc:creator>
      <dc:date>2021-01-22T18:27:31Z</dc:date>
    </item>
  </channel>
</rss>