<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>K32 L Series MicrocontrollersのトピックK32L2A USB RAM</title>
    <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/K32L2A-USB-RAM/m-p/1190489#M21</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;On fig.1 with block diagram from K32L2A datasheet is USB RAM with dedicated connection (black line over mux) to USB module.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="k32l2a.gif" style="width: 570px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/131271i3F336C045BDDCD82/image-size/large?v=v2&amp;amp;px=999" role="button" title="k32l2a.gif" alt="k32l2a.gif" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Let say that BDT with EP buffer's are placed in USB RAM. In moment of receiving 64 bytes EP packet (K32L2A as USB device) from master (PC) &lt;STRONG&gt;all&lt;/STRONG&gt; USB module data access will go over that dedicated connection (black line), or USB module will request access also to (non-USB) RAM. If core executing program from (non-USB) RAM that processing some data stored inside (non-USB) RAM, USB module will steal some cycles (due to non-USB RAM access) or not?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Josip&lt;/P&gt;</description>
    <pubDate>Sat, 28 Nov 2020 07:45:10 GMT</pubDate>
    <dc:creator>jh0</dc:creator>
    <dc:date>2020-11-28T07:45:10Z</dc:date>
    <item>
      <title>K32L2A USB RAM</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/K32L2A-USB-RAM/m-p/1190489#M21</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;On fig.1 with block diagram from K32L2A datasheet is USB RAM with dedicated connection (black line over mux) to USB module.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="k32l2a.gif" style="width: 570px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/131271i3F336C045BDDCD82/image-size/large?v=v2&amp;amp;px=999" role="button" title="k32l2a.gif" alt="k32l2a.gif" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Let say that BDT with EP buffer's are placed in USB RAM. In moment of receiving 64 bytes EP packet (K32L2A as USB device) from master (PC) &lt;STRONG&gt;all&lt;/STRONG&gt; USB module data access will go over that dedicated connection (black line), or USB module will request access also to (non-USB) RAM. If core executing program from (non-USB) RAM that processing some data stored inside (non-USB) RAM, USB module will steal some cycles (due to non-USB RAM access) or not?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Josip&lt;/P&gt;</description>
      <pubDate>Sat, 28 Nov 2020 07:45:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/K32L2A-USB-RAM/m-p/1190489#M21</guid>
      <dc:creator>jh0</dc:creator>
      <dc:date>2020-11-28T07:45:10Z</dc:date>
    </item>
  </channel>
</rss>