<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Device Boot Mode sequence for K32L2B31VFM0A in K32 L Series Microcontrollers</title>
    <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Device-Boot-Mode-sequence-for-K32L2B31VFM0A/m-p/1188862#M20</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;can you provide a low-level time period for the BootCFG[NMI] pin?&lt;/P&gt;</description>
    <pubDate>Wed, 25 Nov 2020 10:07:02 GMT</pubDate>
    <dc:creator>Nikunj</dc:creator>
    <dc:date>2020-11-25T10:07:02Z</dc:date>
    <item>
      <title>Device Boot Mode sequence for K32L2B31VFM0A</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Device-Boot-Mode-sequence-for-K32L2B31VFM0A/m-p/1188211#M18</link>
      <description>&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;Can you provide a Boot Mode sequence timing diagram? if not possible then please suggest how much time we have to put a logic low level on reset and boot config[NMI] pin.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Nikunj&lt;/P&gt;</description>
      <pubDate>Tue, 24 Nov 2020 13:13:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Device-Boot-Mode-sequence-for-K32L2B31VFM0A/m-p/1188211#M18</guid>
      <dc:creator>Nikunj</dc:creator>
      <dc:date>2020-11-24T13:13:50Z</dc:date>
    </item>
    <item>
      <title>Re: Device Boot Mode sequence for K32L2B31VFM0A</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Device-Boot-Mode-sequence-for-K32L2B31VFM0A/m-p/1188718#M19</link>
      <description>&lt;P&gt;Hi Nikunj,&lt;/P&gt;
&lt;P&gt;Reset has two type, POR reset and other reset source reset, include reset pin reset.&lt;/P&gt;
&lt;P&gt;If it's a POR reset, you'd better keep reset pin low till VDD arrive at 1.8V, 1.54v at least. After that LVD will hold reset signal till 1.8V.&amp;nbsp;After a POR event, amount of time from the point VDD reaches 1.8 V to execution of the first instruction is 300us.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jingpan_0-1606290253240.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/130938i98FD5184BD2B8551/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jingpan_0-1606290253240.png" alt="jingpan_0-1606290253240.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If it's a reset pin reset,&amp;nbsp; reset pin should be hold over 1 bus clock. Reset pin can use filter. Please see 6.2.2.1.1 in reference manual.&lt;/P&gt;
&lt;P&gt;To make system stable, you should pull-up reset pin with a 4.7k~10k resistor. And don't connect capacitor to NMI pin.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Wed, 25 Nov 2020 07:48:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Device-Boot-Mode-sequence-for-K32L2B31VFM0A/m-p/1188718#M19</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2020-11-25T07:48:23Z</dc:date>
    </item>
    <item>
      <title>Re: Device Boot Mode sequence for K32L2B31VFM0A</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Device-Boot-Mode-sequence-for-K32L2B31VFM0A/m-p/1188862#M20</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;can you provide a low-level time period for the BootCFG[NMI] pin?&lt;/P&gt;</description>
      <pubDate>Wed, 25 Nov 2020 10:07:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Device-Boot-Mode-sequence-for-K32L2B31VFM0A/m-p/1188862#M20</guid>
      <dc:creator>Nikunj</dc:creator>
      <dc:date>2020-11-25T10:07:02Z</dc:date>
    </item>
    <item>
      <title>Re: Device Boot Mode sequence for K32L2B31VFM0A</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Device-Boot-Mode-sequence-for-K32L2B31VFM0A/m-p/1190501#M22</link>
      <description>&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;we are using 9600&amp;nbsp;baudrate&amp;nbsp;for UART. There is no application firmware inside the device,we observe that if firmware loading is stopped due to some issue we have to always erase the device using j link flash. Then after we receive a valid ping response and the firmware loading is complete inside the device.&lt;/P&gt;&lt;P&gt;Please suggest how to resume firmware load in the device if in boot mode using host((nRF52840) the first time.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;-Nikunj&lt;/P&gt;</description>
      <pubDate>Sat, 28 Nov 2020 08:31:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Device-Boot-Mode-sequence-for-K32L2B31VFM0A/m-p/1190501#M22</guid>
      <dc:creator>Nikunj</dc:creator>
      <dc:date>2020-11-28T08:31:07Z</dc:date>
    </item>
  </channel>
</rss>