<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: STM32L4 having BTstack integrated specific to nxp chipset is having transport layer issues in K32 L Series Microcontrollers</title>
    <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/STM32L4-having-BTstack-integrated-specific-to-nxp-chipset-is/m-p/1848305#M174</link>
    <description>&lt;P&gt;Hello Vidhi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Do you have a complete HCI log? Not just what your host is doing.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
    <pubDate>Tue, 16 Apr 2024 16:20:34 GMT</pubDate>
    <dc:creator>Ricardo_Zamora</dc:creator>
    <dc:date>2024-04-16T16:20:34Z</dc:date>
    <item>
      <title>STM32L4 having BTstack integrated specific to nxp chipset is having transport layer issues</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/STM32L4-having-BTstack-integrated-specific-to-nxp-chipset-is/m-p/1842429#M168</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using the STM32L4 series of controllers which has the BTstack integrated from the BlueKichen. This controller is used to communicate with the CMP530&amp;nbsp;BLE chip which is running on a specific firmware suggested by its chip vendor (CEL).&amp;nbsp;Both the chips are communicating over the UART.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I execute the code in STM with the logs enabled, I can see the below operations performing.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Enabled BLE power&lt;BR /&gt;Init the memory of bt stack&lt;BR /&gt;BTStack Run loop complete&lt;BR /&gt;HCI dump init done&lt;BR /&gt;HCI init done&lt;BR /&gt;HCI set chipset as NXP&lt;BR /&gt;Inside BT stack main&lt;BR /&gt;Event Callback named 'package handler' registered&lt;BR /&gt;Added event handler&lt;BR /&gt;hci_power_control: 1, current mode 0&lt;BR /&gt;state - HCI_STATE_OFF&lt;BR /&gt;Creating internal event&lt;BR /&gt;BTSTACK_EVENT_STATE 1&lt;BR /&gt;[00:00:00.787] EVT &amp;lt;= 60 01 01&lt;BR /&gt;Packet handler state = 0&lt;BR /&gt;Inside INIT&lt;BR /&gt;get state = 01&lt;BR /&gt;HCI packet state = HCI_STATE_INITIALIZING&lt;BR /&gt;hci_initializing_run: substate 0, can send 1&lt;BR /&gt;[00:00:00.806] CMD =&amp;gt; 03 0C 00&lt;BR /&gt;Powered up the HCI&lt;BR /&gt;hci_transport_h4: invalid packet type 0x00&lt;BR /&gt;Resend HCI Reset&lt;BR /&gt;hci_initializing_run: substate 0, can send 0&lt;BR /&gt;&lt;STRONG&gt;hci_can_send_command_packet_now failed&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;From the above logs, it seems like the Transport layer of HCI is not successfully up due to which any packets being sent further are showing the error as above.&lt;/P&gt;&lt;P&gt;As a part of the initial debugging check, I have verified the UART configuration for STM32 on which both chips will communicate. The baud rate is set to 115200 for HCI communication over the UART.&lt;/P&gt;&lt;P&gt;Can anyone please help us to understand what can be the possible reasons behind this?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Vidhi V.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Apr 2024 12:37:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/STM32L4-having-BTstack-integrated-specific-to-nxp-chipset-is/m-p/1842429#M168</guid>
      <dc:creator>Vidhi_V</dc:creator>
      <dc:date>2024-04-08T12:37:38Z</dc:date>
    </item>
    <item>
      <title>Re: STM32L4 having BTstack integrated specific to nxp chipset is having transport layer issues</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/STM32L4-having-BTstack-integrated-specific-to-nxp-chipset-is/m-p/1847343#M172</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. Could you please clarify what is the specific firmware that was suggested by the Module Maker?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;By any chance, do you have some HCI logs?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Mon, 15 Apr 2024 17:22:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/STM32L4-having-BTstack-integrated-specific-to-nxp-chipset-is/m-p/1847343#M172</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2024-04-15T17:22:57Z</dc:date>
    </item>
    <item>
      <title>Re: STM32L4 having BTstack integrated specific to nxp chipset is having transport layer issues</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/STM32L4-having-BTstack-integrated-specific-to-nxp-chipset-is/m-p/1847810#M173</link>
      <description>&lt;P&gt;The vendor of the CMP530 chip has suggested the firmware having HCI interface support. The logs I have dumped above are the logs common out after integrating the BLE Stack.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you mean the HCI logs from the CMP530 chip end? If so, we do not have access to directly check the chip in debug mode and inspect it. We have enabled the HCI logs from the MCU end based on the BTstack that is integrated. The above logs are of the same.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;LEt me know if I can help to get further details.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Vidhi V.&lt;/P&gt;</description>
      <pubDate>Tue, 16 Apr 2024 07:17:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/STM32L4-having-BTstack-integrated-specific-to-nxp-chipset-is/m-p/1847810#M173</guid>
      <dc:creator>Vidhi_V</dc:creator>
      <dc:date>2024-04-16T07:17:04Z</dc:date>
    </item>
    <item>
      <title>Re: STM32L4 having BTstack integrated specific to nxp chipset is having transport layer issues</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/STM32L4-having-BTstack-integrated-specific-to-nxp-chipset-is/m-p/1848305#M174</link>
      <description>&lt;P&gt;Hello Vidhi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Do you have a complete HCI log? Not just what your host is doing.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Tue, 16 Apr 2024 16:20:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/STM32L4-having-BTstack-integrated-specific-to-nxp-chipset-is/m-p/1848305#M174</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2024-04-16T16:20:34Z</dc:date>
    </item>
  </channel>
</rss>