<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>K32 L Series Microcontrollers中的主题 Mcu link SWD Debugging Issues</title>
    <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Mcu-link-SWD-Debugging-Issues/m-p/1782720#M162</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hello.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using the K32L2B21 series&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm going to communicate with mcu link and mcu through SWD&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;On the circuit, the mcu is powered by an LDO of 1.8V&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;(MCU supply power must be 1.8 V)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I understand that mcu link provides 3.3V power&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm trying to do a swd debug, what should I do?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 04 Jan 2024 06:16:04 GMT</pubDate>
    <dc:creator>sw1234</dc:creator>
    <dc:date>2024-01-04T06:16:04Z</dc:date>
    <item>
      <title>Mcu link SWD Debugging Issues</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Mcu-link-SWD-Debugging-Issues/m-p/1782720#M162</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using the K32L2B21 series&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm going to communicate with mcu link and mcu through SWD&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;On the circuit, the mcu is powered by an LDO of 1.8V&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;(MCU supply power must be 1.8 V)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I understand that mcu link provides 3.3V power&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm trying to do a swd debug, what should I do?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jan 2024 06:16:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Mcu-link-SWD-Debugging-Issues/m-p/1782720#M162</guid>
      <dc:creator>sw1234</dc:creator>
      <dc:date>2024-01-04T06:16:04Z</dc:date>
    </item>
    <item>
      <title>Re: Mcu link SWD Debugging Issues</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Mcu-link-SWD-Debugging-Issues/m-p/1844811#M169</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Of course, the MCU-LINK device supports 1.8V logic, but you have change the default configuration on the MCU-LINK probe device.&lt;/P&gt;
&lt;P&gt;1)R16 may be removed&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2) SJ1 changed to connect to position 1-2&lt;/P&gt;
&lt;P&gt;3)The pin1 of J6 must provide 1.8V voltage driven from target board as a reference voltage on the MCU-LINK probe board&lt;/P&gt;
&lt;P&gt;Pls refer to section 5.1&lt;/P&gt;
&lt;P&gt;5.1 Target operating voltage and connections&lt;BR /&gt;The MCU-Link Base Probe cannot power a target system, so uses a sensing circuit (see page 4 of the schematic) to detect the target supply voltage and set up level shifter voltages accordingly. It should not be necessary to make any modifications to this circuit, but there is a pull up resistor (33kΩ) to the 3.3V supply of the MCU-Link. If issues are seen with the target system supply being affected by the MCU-Link being connected then R16 may be removed and SJ1 changed to connect to position 1-2. This will fix the level shifters at the voltage level seen at pin 1 of the SWD connector, and require that the target supply can support the VCCB input requirements of the level shifter devices. It is not recommended to make these modifications until/unless the target system has been carefully checked to see that the correct reference/supply voltage is present on pin 1 of the SWD connector (J6).&lt;/P&gt;
&lt;P&gt;i attach UM11931.pdf&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 11 Apr 2024 05:58:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Mcu-link-SWD-Debugging-Issues/m-p/1844811#M169</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-04-11T05:58:17Z</dc:date>
    </item>
  </channel>
</rss>