<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>K32 L Series MicrocontrollersのトピックUsing both 32 kHz and 8 MHz crystals?</title>
    <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Using-both-32-kHz-and-8-MHz-crystals/m-p/1181644#M16</link>
    <description>&lt;P&gt;On the K32L2A4S I am confused by its oscillator set up in regards to external crystals.&lt;BR /&gt;&lt;BR /&gt;The FRDM-K32L2A4S has a 32 kHz crystal on the EXTAL/XTAL pins for the RTC.&lt;BR /&gt;&lt;BR /&gt;The data sheet says that the minimum input to the PLL is 8 MHz.&lt;BR /&gt;&lt;BR /&gt;What do you need to do if you want an accurate RTC, for when the system is sleeping, and a accurate system clock when running, when not connected to USB?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;From the data sheet and Reference Manual it looks like you can connect a 32 kHz OR a 8 MHz (or higher) crystal, but not both at the same time as they are both on (E)Xtal.&lt;BR /&gt;&lt;BR /&gt;Is there a way to trim the internal osc. with the 32 kHz crystal, like can be done with the AVR?:&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"AVR055: Using a 32kHz XTAL for run-time calibration of the internal RC Osc."&lt;BR /&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="https://www.microchip.com//wwwAppNotes/AppNotes.aspx?appnote=en591195" target="_blank"&gt;https://www.microchip.com//wwwAppNotes/AppNotes.aspx?appnote=en591195&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 11 Nov 2020 19:01:38 GMT</pubDate>
    <dc:creator>bobpaddock</dc:creator>
    <dc:date>2020-11-11T19:01:38Z</dc:date>
    <item>
      <title>Using both 32 kHz and 8 MHz crystals?</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Using-both-32-kHz-and-8-MHz-crystals/m-p/1181644#M16</link>
      <description>&lt;P&gt;On the K32L2A4S I am confused by its oscillator set up in regards to external crystals.&lt;BR /&gt;&lt;BR /&gt;The FRDM-K32L2A4S has a 32 kHz crystal on the EXTAL/XTAL pins for the RTC.&lt;BR /&gt;&lt;BR /&gt;The data sheet says that the minimum input to the PLL is 8 MHz.&lt;BR /&gt;&lt;BR /&gt;What do you need to do if you want an accurate RTC, for when the system is sleeping, and a accurate system clock when running, when not connected to USB?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;From the data sheet and Reference Manual it looks like you can connect a 32 kHz OR a 8 MHz (or higher) crystal, but not both at the same time as they are both on (E)Xtal.&lt;BR /&gt;&lt;BR /&gt;Is there a way to trim the internal osc. with the 32 kHz crystal, like can be done with the AVR?:&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"AVR055: Using a 32kHz XTAL for run-time calibration of the internal RC Osc."&lt;BR /&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="https://www.microchip.com//wwwAppNotes/AppNotes.aspx?appnote=en591195" target="_blank"&gt;https://www.microchip.com//wwwAppNotes/AppNotes.aspx?appnote=en591195&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Nov 2020 19:01:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Using-both-32-kHz-and-8-MHz-crystals/m-p/1181644#M16</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2020-11-11T19:01:38Z</dc:date>
    </item>
  </channel>
</rss>