<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>K32 L Series MicrocontrollersのトピックBulk Out interrupt not working</title>
    <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Bulk-Out-interrupt-not-working/m-p/1768904#M157</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using K32L2A31VLH1A controller for USB. I am configuring USB as CDC class in that CIC for interrupt IN mechanism and DIC for BULK IN/OUT mechanism.&lt;/P&gt;&lt;P&gt;In the code the data which i am writing in console is not coming to device. i debug and check that &amp;nbsp;(USB_DeviceCdcAcmBulkOut) this callback function is not even hitting.&lt;/P&gt;&lt;P&gt;I verified that&amp;nbsp; (USB_DeviceCdcAcmInterruptIn) this callback function is working but not the above callback.&lt;/P&gt;&lt;P&gt;i don't know the reason. Need some help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Tue, 05 Dec 2023 09:17:25 GMT</pubDate>
    <dc:creator>Anirudh_007</dc:creator>
    <dc:date>2023-12-05T09:17:25Z</dc:date>
    <item>
      <title>Bulk Out interrupt not working</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Bulk-Out-interrupt-not-working/m-p/1768904#M157</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using K32L2A31VLH1A controller for USB. I am configuring USB as CDC class in that CIC for interrupt IN mechanism and DIC for BULK IN/OUT mechanism.&lt;/P&gt;&lt;P&gt;In the code the data which i am writing in console is not coming to device. i debug and check that &amp;nbsp;(USB_DeviceCdcAcmBulkOut) this callback function is not even hitting.&lt;/P&gt;&lt;P&gt;I verified that&amp;nbsp; (USB_DeviceCdcAcmInterruptIn) this callback function is working but not the above callback.&lt;/P&gt;&lt;P&gt;i don't know the reason. Need some help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 05 Dec 2023 09:17:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Bulk-Out-interrupt-not-working/m-p/1768904#M157</guid>
      <dc:creator>Anirudh_007</dc:creator>
      <dc:date>2023-12-05T09:17:25Z</dc:date>
    </item>
    <item>
      <title>Re: Bulk Out interrupt not working</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Bulk-Out-interrupt-not-working/m-p/1965085#M235</link>
      <description>&lt;BLOCKQUOTE&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using K32L2A31VLH1A controller for USB. I am configuring USB as CDC class in that CIC for interrupt IN mechanism and DIC for BULK IN/OUT mechanism.&lt;/P&gt;&lt;P&gt;In the code the data which i am writing in console is not coming to device. i debug and check that &amp;nbsp;(USB_DeviceCdcAcmBulkOut) this callback function is not even hitting.&lt;/P&gt;&lt;P&gt;I verified that&amp;nbsp; (USB_DeviceCdcAcmInterruptIn) this callback function is working but not the above callback.&lt;/P&gt;&lt;P&gt;i don't know the reason. Need some help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;If you're encountering an issue with the Bulk Out callback not being triggered in your USB CDC class implementation. First, ensure that your USB endpoint configuration is correct for Bulk Out in both the device and host. Double-check that the USB host is sending data to the correct Bulk Out endpoint and that the endpoint size matches your settings. Hope! it will be helpful.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Oct 2024 10:00:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Bulk-Out-interrupt-not-working/m-p/1965085#M235</guid>
      <dc:creator>harybarok</dc:creator>
      <dc:date>2024-10-01T10:00:13Z</dc:date>
    </item>
    <item>
      <title>Re: Bulk Out interrupt not working</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Bulk-Out-interrupt-not-working/m-p/2328904#M395</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226590"&gt;@Anirudh_007&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you still have question about this case, please feel free to contact me, thank you.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 09 Mar 2026 10:17:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Bulk-Out-interrupt-not-working/m-p/2328904#M395</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2026-03-09T10:17:59Z</dc:date>
    </item>
  </channel>
</rss>