<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Bootloader Development for K32L2B31VFM0A in K32 L Series Microcontrollers</title>
    <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Bootloader-Development-for-K32L2B31VFM0A/m-p/1179411#M15</link>
    <description>&lt;P&gt;UART SERIAL BOOTLOADER FOR K32L2B31VFM0A&lt;/P&gt;&lt;P&gt;I'm using the target device as a K32L2B31VFM0A and the host device as an Nrf52840 microcontroller.&lt;/P&gt;&lt;P&gt;I want to perform an application firmware upgrade of the target device( K32L2B31VFM0A) from the host microcontroller (nRF52840).&lt;/P&gt;&lt;P&gt;I'm using only four pins for the serial bootloader.&lt;/P&gt;&lt;P&gt;LPUART0_RX -Prot PTA1&lt;/P&gt;&lt;P&gt;LPUART0_TX - Port PTA2&lt;/P&gt;&lt;P&gt;NMI_b (BOOTCFG0) - Port PAT4&lt;/P&gt;&lt;P&gt;Reset -Port PTA20&lt;/P&gt;&lt;P&gt;Question 1: can you provide entry boot sequance using boot config pin?&lt;BR /&gt;Question 2: can you please give suggestions on how to do it?&lt;BR /&gt;Question 3: I have to download the host application firmware file (blhost_2.6.2.zip) but this source is in.cpp, so can you provide source code in.c file.?&lt;BR /&gt;Question 4: As per attached screen shot write memory command howmany byte write at a time?,can you provide TX and RX frame format of memory command(in documment example generic frame format not match)?&lt;BR /&gt;Question 5: data command support 32byte only,we are using UART periphiral can we increse data packet byte length.?&lt;BR /&gt;Question 6: Firmware upgrade resume possible? can you provide step?&lt;BR /&gt;Question 7: How to know host device application file write is ok ..App CRC command is supported for this controller?&lt;/P&gt;</description>
    <pubDate>Fri, 06 Nov 2020 11:52:24 GMT</pubDate>
    <dc:creator>kadam</dc:creator>
    <dc:date>2020-11-06T11:52:24Z</dc:date>
    <item>
      <title>Bootloader Development for K32L2B31VFM0A</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Bootloader-Development-for-K32L2B31VFM0A/m-p/1179411#M15</link>
      <description>&lt;P&gt;UART SERIAL BOOTLOADER FOR K32L2B31VFM0A&lt;/P&gt;&lt;P&gt;I'm using the target device as a K32L2B31VFM0A and the host device as an Nrf52840 microcontroller.&lt;/P&gt;&lt;P&gt;I want to perform an application firmware upgrade of the target device( K32L2B31VFM0A) from the host microcontroller (nRF52840).&lt;/P&gt;&lt;P&gt;I'm using only four pins for the serial bootloader.&lt;/P&gt;&lt;P&gt;LPUART0_RX -Prot PTA1&lt;/P&gt;&lt;P&gt;LPUART0_TX - Port PTA2&lt;/P&gt;&lt;P&gt;NMI_b (BOOTCFG0) - Port PAT4&lt;/P&gt;&lt;P&gt;Reset -Port PTA20&lt;/P&gt;&lt;P&gt;Question 1: can you provide entry boot sequance using boot config pin?&lt;BR /&gt;Question 2: can you please give suggestions on how to do it?&lt;BR /&gt;Question 3: I have to download the host application firmware file (blhost_2.6.2.zip) but this source is in.cpp, so can you provide source code in.c file.?&lt;BR /&gt;Question 4: As per attached screen shot write memory command howmany byte write at a time?,can you provide TX and RX frame format of memory command(in documment example generic frame format not match)?&lt;BR /&gt;Question 5: data command support 32byte only,we are using UART periphiral can we increse data packet byte length.?&lt;BR /&gt;Question 6: Firmware upgrade resume possible? can you provide step?&lt;BR /&gt;Question 7: How to know host device application file write is ok ..App CRC command is supported for this controller?&lt;/P&gt;</description>
      <pubDate>Fri, 06 Nov 2020 11:52:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Bootloader-Development-for-K32L2B31VFM0A/m-p/1179411#M15</guid>
      <dc:creator>kadam</dc:creator>
      <dc:date>2020-11-06T11:52:24Z</dc:date>
    </item>
  </channel>
</rss>