<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Serial bootloder for K32L2B31VFM0A in K32 L Series Microcontrollers</title>
    <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Serial-bootloder-for-K32L2B31VFM0A/m-p/1173795#M13</link>
    <description>&lt;P&gt;hello,&lt;/P&gt;&lt;P&gt;I have to download the host application firmware file (blhost_2.6.2.zip) but this source is in.cpp, so can you provide source code in.c file.&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;-Nikunj&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 27 Oct 2020 11:08:31 GMT</pubDate>
    <dc:creator>Nikunj</dc:creator>
    <dc:date>2020-10-27T11:08:31Z</dc:date>
    <item>
      <title>Serial bootloder for K32L2B31VFM0A</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Serial-bootloder-for-K32L2B31VFM0A/m-p/1173093#M12</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using the target device as a&amp;nbsp;K32L2B31VFM0A and the host device as an Nrf52840 microcontroller.&lt;/P&gt;&lt;P&gt;I want to perform an application firmware upgrade of the target device(&amp;nbsp;K32L2B31VFM0A) from the host microcontroller (nRF52840).&lt;/P&gt;&lt;P&gt;I'm using only four pins for the serial bootloader.&lt;/P&gt;&lt;P&gt;LPUART0_RX&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;-Prot PTA1&lt;/P&gt;&lt;P&gt;LPUART0_TX&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;- Port PTA2&lt;/P&gt;&lt;P&gt;NMI_b (BOOTCFG0)&amp;nbsp; &amp;nbsp;- Port PAT4&lt;/P&gt;&lt;P&gt;Reset&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -Port PTA20&amp;nbsp;&lt;/P&gt;&lt;P&gt;can you please give suggestions on how to do it?&lt;/P&gt;</description>
      <pubDate>Mon, 26 Oct 2020 11:34:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Serial-bootloder-for-K32L2B31VFM0A/m-p/1173093#M12</guid>
      <dc:creator>Nikunj</dc:creator>
      <dc:date>2020-10-26T11:34:49Z</dc:date>
    </item>
    <item>
      <title>Re: Serial bootloder for K32L2B31VFM0A</title>
      <link>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Serial-bootloder-for-K32L2B31VFM0A/m-p/1173795#M13</link>
      <description>&lt;P&gt;hello,&lt;/P&gt;&lt;P&gt;I have to download the host application firmware file (blhost_2.6.2.zip) but this source is in.cpp, so can you provide source code in.c file.&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;-Nikunj&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Oct 2020 11:08:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/K32-L-Series-Microcontrollers/Serial-bootloder-for-K32L2B31VFM0A/m-p/1173795#M13</guid>
      <dc:creator>Nikunj</dc:creator>
      <dc:date>2020-10-27T11:08:31Z</dc:date>
    </item>
  </channel>
</rss>