<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUs中的主题 Re: IMXRT1050 Using both USB Host and USB Device</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1050-Using-both-USB-Host-and-USB-Device/m-p/1088501#M9471</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case there remains problems with dual-USB operation you can take a look at the uTasker project which allows code to run on Kinetis and i.MX RT parts with single or dual-USB.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The following short video shows the same project running on a Teensy 3.6 (K66F with FS and HS USB) and on an i.MX RT 1060 with USB-CDC on the first HS USB and MSD host (memory stick) on the second.&lt;BR /&gt;The complete USB controller operation and memory stick are also simulated so that development and debugging becomes much easier and more fun!&lt;BR /&gt;No porting between parts is needed and dual HS USB runs on i.MX RT 1050, i.MX 1060 and i.MX RT 1064 in any combination: device + host, host + device, 2 x device, or 2 x host.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://youtu.be/3irORtbc4e0" target="test_blank"&gt;https://youtu.be/3irORtbc4e0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;&lt;EM&gt;[uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Jun 2020 22:39:57 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2020-06-12T22:39:57Z</dc:date>
    <item>
      <title>IMXRT1050 Using both USB Host and USB Device</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1050-Using-both-USB-Host-and-USB-Device/m-p/1088500#M9470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to get both USB device and USB host working on my board, USB host will have a MSD attached to it and USB Device will connect to the computer. I took the USB dev_cdc_vcom_freertos demo and tried to add it to the host_msd_freertos demo (With fatfs ported into it). After making some changes I got my project to build but I am having trouble with the USB device, I keep getting this error when I connect it "ASSERT ERROR " .fsl_os_abstraction_free_rtos.c:625 : pdPASS == result". As well USB Host does not complete any of the file server commands. Any suggestions on how to get the two USB's working together?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2020 19:49:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1050-Using-both-USB-Host-and-USB-Device/m-p/1088500#M9470</guid>
      <dc:creator>nicole1</dc:creator>
      <dc:date>2020-06-11T19:49:27Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1050 Using both USB Host and USB Device</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1050-Using-both-USB-Host-and-USB-Device/m-p/1088501#M9471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case there remains problems with dual-USB operation you can take a look at the uTasker project which allows code to run on Kinetis and i.MX RT parts with single or dual-USB.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The following short video shows the same project running on a Teensy 3.6 (K66F with FS and HS USB) and on an i.MX RT 1060 with USB-CDC on the first HS USB and MSD host (memory stick) on the second.&lt;BR /&gt;The complete USB controller operation and memory stick are also simulated so that development and debugging becomes much easier and more fun!&lt;BR /&gt;No porting between parts is needed and dual HS USB runs on i.MX RT 1050, i.MX 1060 and i.MX RT 1064 in any combination: device + host, host + device, 2 x device, or 2 x host.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://youtu.be/3irORtbc4e0" target="test_blank"&gt;https://youtu.be/3irORtbc4e0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;&lt;EM&gt;[uTasker project developer for Kinetis and i.MX RT]&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jun 2020 22:39:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/IMXRT1050-Using-both-USB-Host-and-USB-Device/m-p/1088501#M9471</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2020-06-12T22:39:57Z</dc:date>
    </item>
  </channel>
</rss>