<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRT1064: does SWO trace need external component?</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-does-SWO-trace-need-external-component/m-p/1069500#M8716</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For RT1064,&amp;nbsp;I would like to use the SWO trace function, located on pin GPIO_AD_B0_10.&amp;nbsp; Does this require any external component such as pull-up or pull-down resistor?&amp;nbsp; I do not see this information anywhere in RT1064 documentation.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The reason I ask is because on RT1064 EVK, GPIO_AD_B0_10 is used as an interrupt signal for Ethernet (net "ENET_INT") which has a 1k pull-up resistor on it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jason&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Aug 2020 10:04:15 GMT</pubDate>
    <dc:creator>jason_lo</dc:creator>
    <dc:date>2020-08-26T10:04:15Z</dc:date>
    <item>
      <title>RT1064: does SWO trace need external component?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-does-SWO-trace-need-external-component/m-p/1069500#M8716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For RT1064,&amp;nbsp;I would like to use the SWO trace function, located on pin GPIO_AD_B0_10.&amp;nbsp; Does this require any external component such as pull-up or pull-down resistor?&amp;nbsp; I do not see this information anywhere in RT1064 documentation.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The reason I ask is because on RT1064 EVK, GPIO_AD_B0_10 is used as an interrupt signal for Ethernet (net "ENET_INT") which has a 1k pull-up resistor on it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jason&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2020 10:04:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-does-SWO-trace-need-external-component/m-p/1069500#M8716</guid>
      <dc:creator>jason_lo</dc:creator>
      <dc:date>2020-08-26T10:04:15Z</dc:date>
    </item>
    <item>
      <title>Re: RT1064: does SWO trace need external component?</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-does-SWO-trace-need-external-component/m-p/1132747#M9869</link>
      <description>&lt;P&gt;Hello Jason,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;You may refer to this document for debug considerations. For the SWO you must use a pull-up for better performance.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565" target="_self"&gt;Design-Considerations-for-Debug&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Sabina&lt;/P&gt;</description>
      <pubDate>Mon, 31 Aug 2020 21:50:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1064-does-SWO-trace-need-external-component/m-p/1132747#M9869</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2020-08-31T21:50:16Z</dc:date>
    </item>
  </channel>
</rss>