<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX RT Crossover MCUsのトピックRe: SDRAM Bootable Image</title>
    <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SDRAM-Bootable-Image/m-p/1066562#M8632</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello James,&lt;/P&gt;&lt;P&gt;Hope you are doing well.&lt;/P&gt;&lt;P&gt;I recommend to begin with the following document:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-340655"&gt;https://community.nxp.com/docs/DOC-340655&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It provides the steps necessary to create the bootable image for sdram.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Aug 2020 19:09:15 GMT</pubDate>
    <dc:creator>Sabina_Bruce</dc:creator>
    <dc:date>2020-08-07T19:09:15Z</dc:date>
    <item>
      <title>SDRAM Bootable Image</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SDRAM-Bootable-Image/m-p/1066561#M8631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there an example/ guide available for an SDRAM bootable image on the RT1052?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried to convert one of the SDK sample project into SDRAM bootable image but unable to boot from flash&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;SDK example projects (which has ethernet-wifi, LWIP, AWS, and Iot module)&lt;/P&gt;&lt;OL style="margin-top: 0cm;"&gt;&lt;LI style="margin-left: 0cm;"&gt;“evkbimxrt1050_Aws_aws_shadow_wiced&lt;/LI&gt;&lt;LI style="margin-left: 0cm;"&gt;&amp;nbsp;evkbimxrt1050_AWS_aws_greengrass_discovery_enet"&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have noticed, if&amp;nbsp; project is based on the “ethernet / wifi” or LWIP”&amp;nbsp; the SDRAM boot issue arise (irrespective of Flash memory ).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Aug 2020 10:09:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SDRAM-Bootable-Image/m-p/1066561#M8631</guid>
      <dc:creator>james_moore</dc:creator>
      <dc:date>2020-08-05T10:09:53Z</dc:date>
    </item>
    <item>
      <title>Re: SDRAM Bootable Image</title>
      <link>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SDRAM-Bootable-Image/m-p/1066562#M8632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello James,&lt;/P&gt;&lt;P&gt;Hope you are doing well.&lt;/P&gt;&lt;P&gt;I recommend to begin with the following document:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-340655"&gt;https://community.nxp.com/docs/DOC-340655&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It provides the steps necessary to create the bootable image for sdram.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Aug 2020 19:09:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/SDRAM-Bootable-Image/m-p/1066562#M8632</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2020-08-07T19:09:15Z</dc:date>
    </item>
  </channel>
</rss>